Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Schematic not showing all pins on device
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 645 views
  • Users 0 members are here
Related

Schematic not showing all pins on device

e14 Contributor
e14 Contributor over 15 years ago

Hello,

 

I am attempting to use the 74LS373N DIL20 device in the 74xx-us library that you can download from Eagle.  When I add the device to schematic, it shows all pins, except 10 and 20.  I have included pictures to demonstrate what I'm trying to show as the problem.  There are two schematic symbols that are supposed to show up when you add the device to schematic, the data pins, and the power and ground.  It doesn't show the power and ground pins.

 

Can anyone tell me why this is happening?

 

Thanks,

 

-Eric

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 15 years ago

    Hi Eric,

     

    it is possible to create devices that consist of several symbols and you can decide how to place them in the schematic (Addlevel). Lot of devices have the power pins hidden. To get them visible in the schematic use the INVOKE command (it's represented by an icon that shows kind of four gates) and click onto the symbol (or type in its name in the command line). Now you get a table with available gates you can place.

     

    Regards
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 15 years ago

    Hi Eric,

     

    it is possible to create devices that consist of several symbols and you can decide how to place them in the schematic (Addlevel). Lot of devices have the power pins hidden. To get them visible in the schematic use the INVOKE command (it's represented by an icon that shows kind of four gates) and click onto the symbol (or type in its name in the command line). Now you get a table with available gates you can place.

     

    Regards
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to Richard_H

    Thank you Richard, that did the trick!