Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to Remove Pins From a Routed Board Net?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 784 views
  • Users 0 members are here
Related

How to Remove Pins From a Routed Board Net?

e14 Contributor
e14 Contributor over 15 years ago

Hello all,

 

I had submitted this question to Richard in Cadsoft support, but thought I start it as a new discussion as well.  

 

I have a simple issue that I'm stuck on. I've finished routing a four layer board, and somehow managed to connect a chip enable net, N_CE0 to the power plane net, VDD_FLASH.  I need to remove two pins from the power net and recreate the chip enable net.  I've tried deleting the routs and airwires for the chip enable net, and entering the netlist again with no luck.  Can you tell me how to correct my problem?

 

Thanks in advance for any help you can provide.

 

Cheers,

 

Ralph

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Ralph,

    Glad see I was of some help. If you have further question don't hesistate to contact us.  Last year I found a series of tutorials on youtube.com, they work really nice.

     

    YouTube Video Tutorials:
    http://www.youtube.com/watch?v=qG0O9LKH-_E
    http://www.youtube.com/watch?v=z4Io4qZCzYI
    http://www.youtube.com/watch?v=G0bMfV3IbMo
    http://www.youtube.com/watch?v=rGiHdNyHbDM
    http://www.youtube.com/watch?v=3Xj1Xrp8uso
    http://www.youtube.com/watch?v=UW_Jkzuo_mc
    http://www.youtube.com/watch?v=TmV9urSuSFU
    http://www.youtube.com/watch?v=4JC32tq7Ibo
    http://www.youtube.com/watch?v=4xjjahxMapc
    http://www.youtube.com/watch?v=cB5Z_fRpLrE
    http://www.youtube.com/watch?v=tna0XNjHkrw

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hello Ed,

     

    Thanks very much for your suggestions.  I was using a supply layer, and your process of simply unchecking supply in the layer display panel is better than the "rename the supply layer" process I used.  I'm still very new to Eagle, and still learning some of the tool's basic features.

     

    Thanks again.

     

    Cheers,

     

    Ralph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hi,

    I am not sure if the connections are to supply plane or to a polygon, so I will provide you some simple steps you may consider.

    Supply Layer

    If  you are using a supply layer, use the DISPLAY command to view your  layers.  You will notice your internal layer will have the name  $VDD_FLASH.  Double click this layers and disable the SUPPLY option and  click OK and run RATSNEST.  You will now notice the airwire.  In the  schematic, delete the connection and make necessary modifications.  If  you are using a SCRIPT file, delete the connections on the board and  import the script file or use the SIGNAL command to define the  coneection manually.

     

    Polygon

    Type the command RIP @; and press enter.  This will ripup all the polygons and place them in outline form.  Now  click on Options/Set/MISC tab and disable the option 'RATSNEST PROCESSES  POLYGONS'.

    Now run the RATSNETS command. You will notice the the  implicit airwires appear since the polygon no longer pours.  Make the  appropiate changes to the schematic.  If not, delete the connections on  the board and import the netscript.

    I hope this helps.

    Best Regards,

    Ed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hello all,

     

    I believe I found a solution to the problem I created using the following process:

    1. I renamed the power plane from VDD_FLASH to  _VDD_FLASH which removed all of the power plane connections.

    2. I then ripped up the traces leading to the two pins I needed to remove from the power net.

    3. I then deleted the airwires going to those two pins.

    4. Saved the job file.

    5. Reran the script to reload the netlist into the board.

    6. Ran the ratnest command and confirmed that the airwire for the two pins was now the N_CE2 net.

    7. Renamed the power plane back to VDD_FLASH and ran DRC.

    8. Rerouted the N_CE2 net, ran DRC, and verified that the net is still the N_CE2 net name.

     

    I'll export the netlist from the board to verify that the netlist matches the script, but this does appear to have fixed the problem.  The trick appeared to be renaming the power plane to remove the automatic connections, so I could rip up the part of the net I needed to isolate.

     

    Cheers,

     

    Ralph