Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to Remove Pins From a Routed Board Net?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 782 views
  • Users 0 members are here
Related

How to Remove Pins From a Routed Board Net?

e14 Contributor
e14 Contributor over 15 years ago

Hello all,

 

I had submitted this question to Richard in Cadsoft support, but thought I start it as a new discussion as well.  

 

I have a simple issue that I'm stuck on. I've finished routing a four layer board, and somehow managed to connect a chip enable net, N_CE0 to the power plane net, VDD_FLASH.  I need to remove two pins from the power net and recreate the chip enable net.  I've tried deleting the routs and airwires for the chip enable net, and entering the netlist again with no luck.  Can you tell me how to correct my problem?

 

Thanks in advance for any help you can provide.

 

Cheers,

 

Ralph

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hi,

    I am not sure if the connections are to supply plane or to a polygon, so I will provide you some simple steps you may consider.

    Supply Layer

    If  you are using a supply layer, use the DISPLAY command to view your  layers.  You will notice your internal layer will have the name  $VDD_FLASH.  Double click this layers and disable the SUPPLY option and  click OK and run RATSNEST.  You will now notice the airwire.  In the  schematic, delete the connection and make necessary modifications.  If  you are using a SCRIPT file, delete the connections on the board and  import the script file or use the SIGNAL command to define the  coneection manually.

     

    Polygon

    Type the command RIP @; and press enter.  This will ripup all the polygons and place them in outline form.  Now  click on Options/Set/MISC tab and disable the option 'RATSNEST PROCESSES  POLYGONS'.

    Now run the RATSNETS command. You will notice the the  implicit airwires appear since the polygon no longer pours.  Make the  appropiate changes to the schematic.  If not, delete the connections on  the board and import the netscript.

    I hope this helps.

    Best Regards,

    Ed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hi,

    I am not sure if the connections are to supply plane or to a polygon, so I will provide you some simple steps you may consider.

    Supply Layer

    If  you are using a supply layer, use the DISPLAY command to view your  layers.  You will notice your internal layer will have the name  $VDD_FLASH.  Double click this layers and disable the SUPPLY option and  click OK and run RATSNEST.  You will now notice the airwire.  In the  schematic, delete the connection and make necessary modifications.  If  you are using a SCRIPT file, delete the connections on the board and  import the script file or use the SIGNAL command to define the  coneection manually.

     

    Polygon

    Type the command RIP @; and press enter.  This will ripup all the polygons and place them in outline form.  Now  click on Options/Set/MISC tab and disable the option 'RATSNEST PROCESSES  POLYGONS'.

    Now run the RATSNETS command. You will notice the the  implicit airwires appear since the polygon no longer pours.  Make the  appropiate changes to the schematic.  If not, delete the connections on  the board and import the netscript.

    I hope this helps.

    Best Regards,

    Ed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hello Ed,

     

    Thanks very much for your suggestions.  I was using a supply layer, and your process of simply unchecking supply in the layer display panel is better than the "rename the supply layer" process I used.  I'm still very new to Eagle, and still learning some of the tool's basic features.

     

    Thanks again.

     

    Cheers,

     

    Ralph