Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Auto-router violates its own rules
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 596 views
  • Users 0 members are here
Related

Auto-router violates its own rules

KE5FX
KE5FX over 15 years ago

Hi -- I'm curious if I've got something configured wrong here.  My impression is that the autorouter will unconditionally obey the rules established in the Tools->DRC and Tools->Auto dialogs, but I'm getting clearance errors on some autorouted tracks.  Is this just a consequence of the routing grid being too coarse?  It's set to 3 mil in this case.  One of many examples is attached, where a 6mm trace/space rule is in effect but the autorouter has placed a track that's clearly less than 6 mm from another feature.

Attachments:
image
image
  • Sign in to reply
  • Cancel
  • Richard_H
    0 Richard_H over 15 years ago in reply to KE5FX

    Hi John,

     

    I think it's only possible for the author to delete the message. But I think it is not a problem to leave it as it is.

    So the community can see that it is not a problem of the autorouter. image

     

    Best regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • KE5FX
    0 KE5FX over 15 years ago in reply to KE5FX

    Actually, never mind this unless/until I can get it to happen again... I'm not 100% sure I saved the file after the last router pass. image  I appear to be loading a version that was routed under legitimate 5mm rules.  Apologies for the false alarm ... this thread should be deleted if a mod can do that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KE5FX
    0 KE5FX over 15 years ago

    (If it matters, this is EAGLE 5.11 Pro.)