Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Can I layout a circular pc board with Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 190 subscribers
  • Views 3560 views
  • Users 0 members are here
Related

Can I layout a circular pc board with Eagle

e14 Contributor
e14 Contributor over 14 years ago

I reviewed the 2 Eagle videos by Jeremy and the board he designed was rectangular. I'm wondering if I could lay out a 3" diameter circular board with Eagle.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    OK Thanks. I see someone made a nice round board here: http://www.element14.com/community/thread/18133?tstart=0 

    The person "created this in eagle with dimension layer round 114mm." Anyone know if this is a command in Eagle to simply set the dimension layer to round?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RayA
    0 RayA over 14 years ago in reply to e14 Contributor

    Rather than making a square board and rounding the corners 100%, I think you would just use the "Circle" command to place a circular outline in layer 20.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RayA

    Thanks.

     

    That's what I was hoping for. Your answer made me download the Eagle manual http://www.cadsoft.de/wp-content/uploads/2011/05/V6_manual_en.pdf and this is what it says on p148:

    "The board outline can be drawn as a simple narrow line in layer 20,

    Dimension with the WIRE command.

    It's easily possible to draw round outlines, too. Therefore use the CIRCLE

    command with a small width near 0.

    You can also place a board contour from a library (such as 19inch.lbr) with

    ADD.

    A script file can, alternatively, be read by the SCRIPT command. The euro.scr

    file, for instance, can be used. Simply type

    SCRIPT EURO

    on the command line.

    The board outline serves simultaneously as a boundary for the autorouter or

    Follow-me router (if present).

    If your board has additional cut-outs, you should draw the necessary milling

    contours in a separate layer, for example in 46, Milling. Use the WIRE

    command with wire width = 0 to define your lines."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RayA
    0 RayA over 14 years ago in reply to e14 Contributor

    You're welcome, Joe.

     

    One other comment is that I use a narrow line line, 0.003" instead of 0.000",  for the board outline and milling cutouts. The reason is that the Eagle software will automatically provide a solid filll to any circles that have a zero width.

    The boardhouse that I usually use cuts to the center of the line, so they don't care if the line is non-zero width.

     

    Maybe someone with more experience can comment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • RayA
    0 RayA over 14 years ago in reply to e14 Contributor

    You're welcome, Joe.

     

    One other comment is that I use a narrow line line, 0.003" instead of 0.000",  for the board outline and milling cutouts. The reason is that the Eagle software will automatically provide a solid filll to any circles that have a zero width.

    The boardhouse that I usually use cuts to the center of the line, so they don't care if the line is non-zero width.

     

    Maybe someone with more experience can comment.