Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum QVSOP80 Footprint for E.A.G.L.E. C.A.D.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 467 views
  • Users 0 members are here
Related

QVSOP80 Footprint for E.A.G.L.E. C.A.D.

e14 Contributor
e14 Contributor over 13 years ago

Just wondering if anyone has an Eagle footprint for the QVSOP-80 package as used by the IDTQS34XVH245 QUICKSWITCHRegistered PRODUCTS 2.5V / 3.3V 32-BIT HIGH BANDWIDTH BUS SWITCH.

Better yet, does anyone have an eagle library part for same? I usually use the eagle reference packages library to create my own parts, however qvsop packages are absent from that footprint library.

I have managed to get the datasheet for the package from IDT and can build the part in eagle. Of course, I need to order some IDTQS34XVH245 to verify my footprint once it is completed. This is for a project that I plan to start the third week or so of January 2013 assuming the world does not end on December the 21st :-) If anyone already has this footprint or a complete part, it would certainly save a bit of time. I should mention that I am still using Eagle 5.xx, but soon plan to upgrade to 6.xx. Many Thanks - John

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Richard_H

    @Richard. Thanks for the suggestion, it is appreciated. I went ahead and created a qvsop80 footprint based on Reference: Jedec Mo-154, Issue C. I do not want to upload it yet, until I verify that it is accurate. However, anyone wishing to have a look at it and perhaps verify it (I haven't received my 32-bit bus switches yet to use for verification), may contact me and I will send the footprint for them to have a look at. I can probably also create similar footprints for anyone in need of a hard to find footprint. Just drop me a message. Regards - John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Richard_H
    0 Richard_H over 13 years ago

    Hi John,

     

    seems as if nobody has such a library available. You could for example write a request to the guys that take care on the EAGLE libraries here on the element14.com wen page. Maybe they can help you. I don't want to promise anything, but it is worth a try....

     

    email to  cad_tech@element14.com

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer