Just wondering if anyone has an Eagle footprint for the QVSOP-80 package as used by the IDTQS34XVH245 QUICKSWITCH PRODUCTS 2.5V / 3.3V 32-BIT HIGH BANDWIDTH BUS SWITCH.
Better yet, does anyone have an eagle library part for same? I usually use the eagle reference packages library to create my own parts, however qvsop packages are absent from that footprint library.
I have managed to get the datasheet for the package from IDT and can build the part in eagle. Of course, I need to order some IDTQS34XVH245 to verify my footprint once it is completed. This is for a project that I plan to start the third week or so of January 2013 assuming the world does not end on December the 21st :-) If anyone already has this footprint or a complete part, it would certainly save a bit of time. I should mention that I am still using Eagle 5.xx, but soon plan to upgrade to 6.xx. Many Thanks - John