Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Merge board/schematic pairs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 2927 views
  • Users 0 members are here
Related

Merge board/schematic pairs

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I read this :

Merge board/schematic pairs using the PASTE function with full consistency

You can copy an already finished design consisting of a consistent pair of Schematic and Layout into another project. Enumeration of components and signals will be exactly the same in board and schematic, so that consistency between schematic and board will be maintained. This supports easy design, for example, of multi-channel devices. You only have to design schematic and layout for one channel and can copy it easily

 

I didn't find any explanation in the V6_manual_en.pdf

 

How can I do this : Merge board/schematic pairs ?

 

Best regards.

Pierre.

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 13 years ago

    Hello,

     

    this can be done through the File/Import menu.

    It is described in the manual: Please look into the section Merge Different Schematic Files in chapter 6.1.

     

    Best regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Richard_H

    Thanks for your prompt response,

     

    I did't find ( edit/paste from ...)  menu or commande

    I must use File/Import ; Eagle drawing ; then I have a new window " paste from file " . Is it the only way to proceed ?

     

    Manual chapter 6.1 ......

    As an alternative to the Edit/Paste from... menu and typing the PASTE

    command into the command line, it is possible to drag&drop a schematic or a

    layout from the treeview's projects branch of the Control Panel into an opened

    Schematic or Layout Editor window.

    It's missing that we must pressing the Ctrl key when dropping the file. ( when you want merge board/schematic pairs )

     

    Another question :

    I have a finish schematic/board pair . For example a schematic/board pair with one preamplifier and one amplifier.

    I want to add on the same board 3 copy of the preamplifier that is already on this pcb (copy and paste the existing preamplifier from Board).

    How can I do that ?

     

    Best regards.

    Pierre

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 13 years ago in reply to e14 Contributor

    Hi Pierre,

     

    I suppose you are working with an EAGLE 6.3.x or 6.4.0? This function has moved into the File/Import... menu. Choose EAGLE drawing there..

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Richard_H

    Hi Richard,

     

    Thanks , yes I am working with EAGLE 6.4.0

     

    Best regards.

    Pierre.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Richard_H

    Hi Richard,

     

    Thanks , yes I am working with EAGLE 6.4.0

     

    Best regards.

    Pierre.