Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Arbitary SMD and DRC frustration
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 730 views
  • Users 0 members are here
  • pads
  • custom_pads
  • arbitary_smd
Related

Arbitary SMD and DRC frustration

e14 Contributor
e14 Contributor over 13 years ago

I have created a footprint for a SON-6 package, quite small.  The datasheet calls for oblong pads 0.28mm wide by 0.75mm long and one end being completely rounded (i.e, r=0.14). I used a polygon with wire width 0 to achieve this as the embedded help file appears to say DRC does not check wire width of polygons used for arbitary pads.  However, DRC is throwing up a width error for these smd pads.  If I thicken the wire width to fit in with my DRC settings I can't create the smd shape I need. Is this a bug in the software or a bug with the way I'm trying to work?  Any feedback other than 'just use rectangular smd pads' is welcome.

 

Thanks, William

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Richard_H

    Thanks for confirming Richard.  So it seems the polygon smd pad function isn't yet up to the job for very small packages - even if I declare a polygon line width of 0.01mm that makes a significant error difference to the area and spacing for my SON-6 footprint.  I guess if I just approve the errors for now and verify the gerber output, that is the only option for me today.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 13 years ago in reply to e14 Contributor

    Hi William,

     

    you have to draw the polygons in a reasonable wire width. If you take 0 as width, there will be additional constraints for the production process. Gerber data usually doesn't accept 0 width data. This is also written in the manual:

     

    8.14 Arbitrary Pad Shapes

    [.........]

    The typical way to draw an arbitrary pads shape is:

    * Place a PAD or SMD

    * Use POLYGON to draw the final pad shape

    For a SMD typically in Layer Top

    For a PAD you have to draw the final shape in all the layers you plan

    to use (Top, Bottom, Inner layers...)

    The PAD/SMDs center must be inside the polygon's area. Otherwise

    that polygon is not recognized as a part to the pad. Use a reasonable 

    wire width for the polygon, which fulfils the Design Rules.

    [........]

     

    I am currently discussing with our development team whether we can change

    this for the future.....

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Richard_H

    Hi Richard,

     

    I sent the library file this morning, did you have a chance to look at it yet?

     

    Thanks

     

    William

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 13 years ago

    Hi William,

     

    could you please send me the library you created. So I could check what the problem is there.

    Please send it to:  support@cadsoft.de

     

    Regards,

    Richard