Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Group Does Not Work
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 520 views
  • Users 0 members are here
Related

Group Does Not Work

e14 Contributor
e14 Contributor over 11 years ago

According to the Manual Version 7, 2nd Edition, page 57, one should be able to use the Ctrl and Shift keys to toggle membership in a defined group:

If you like to add further groups to an already existing one, press the Shift key and define the first corner of the selection area with a mouse click.

 

In case you want to add an object to or remove it from the group, press the Ctrl key and click onto the object in question.

 

Press Ctrl + Shift to toggle the membership of an object and its hierarchically superior objects: Clicking for example, on a net segment in the Schematic

inverts the group membership of the whole net.

 

I cannot get the keys to function as described, either with a real schematic or just a simplified example consisting of 4 capacitors.  What is the trick to get it to work as described?  Is there a video demonstration showing those functions?

 

John

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    OK, I think I got the CTRL key figured out to add or subtract from a group.  A bit clumsy, but it works.  You have to keep re-selecting the group icon.  For example, if you have move selected, then group.  The program reverts to move once the group is selected.  You need to re-select group to add or subtract from the group.  At least, it works with simple objects that have distinctly marked origins.  John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    OK, I think I got the CTRL key figured out to add or subtract from a group.  A bit clumsy, but it works.  You have to keep re-selecting the group icon.  For example, if you have move selected, then group.  The program reverts to move once the group is selected.  You need to re-select group to add or subtract from the group.  At least, it works with simple objects that have distinctly marked origins.  John