Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum INDUSTRIAL LASER DISTANCE SENSOR INTERFACE (PNBC006 WENGLOR)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 186 subscribers
  • Views 1060 views
  • Users 0 members are here
  • PNBC006 WENGLOR troubles RPi interface
Related

INDUSTRIAL LASER DISTANCE SENSOR INTERFACE (PNBC006 WENGLOR)

AZ87
AZ87 over 3 years ago

Hello everybody, let me start by saying that I'm a complete newbie to the world of programming and microcontrollers in general and also new to this Element14 community. I'm here to ask for your help and YOU are my last hope. I am working on a project where a laser distance sensor(precisely the Wenglor PNBC006) will be placed over a car tyre ( at about 200mm) and it will be moving through a slide controlled by a stepper motor along the width of the tyre; this laser basically has to "reproduce" the tyre treading profile by measuring the distance over the tyre  treading itself; my question is : HOW IN THE WORLD DO I GET THE SENSOR READINGS FROM RASPBERRY PI 4 and plot those readings in such a way that I get a continuous line plotted that reproduces the tyre treading profile scanned?

I have been through the documentation of the laser and it mentions that it support 2 kind of connections: M12 8pins cable AND an Ethernet one; from my understanding (based on the docs on the web) i can connect the sensor to a specific Ethernet switch and access the "control panel interface" of the sensor with an IP address which is provided in the Wenglor docs; till I'm ok; but how do I get the readings from the sensor straight to Raspberry pi?!?

Please help me out or point in the right direction! I'm quite disperate since I've also blasbt a couple of emails to the Wenglor assistance 2 weeks ago and did not get any answer back(probably i will never get one because of 'stupid and useless ' question exposing my ignorance!  ..what a frustration!! I really appreciate any information, anything that could potentially point into the right direction.

Here is the sensor 

www.wenglor.com/.../

Here is the official doc

www.wenglor.com/.../__secure__

PLEASE HELP ME OUT 

THANK YOU SO MUCH ALL

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 3 years ago

    This should be deleted, it's got nothing to do with EAGLE.

    It's a duplicate question, answered here:

     PNBC006 WENGLOR DISTANCE LASER SENSOR RPi interfacing trouble