Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum 1.8mm and 3mm through-hole
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 1630 views
  • Users 0 members are here
  • eagle
  • eagle pcb
  • eagle schematic
Related

1.8mm and 3mm through-hole

e14 Contributor
e14 Contributor over 10 years ago

Hi

I am using Eagle Light version and trying to find a library for hole (1.8mm and 3mm in diameter).

I tried using by-default holes.lbr and wirepad.lbr but the diameter for that holes are smaller than requirement.

 

Can somebody help me out? Any help would be highly appreciated.

Regards

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 10 years ago

    Do you want a non-plated or plated through hole? You can just add these in the layout without adding a library part.

     

    In layout do the following commands:

     

    For non-plated holes -

     

    grid mm

    hole 1.8 <click to place>

    hole 3 <click to place>

     

    For plated holes -

     

    grid mm

    via round <click to place>

    change drill 1.8 <click via to change>

    via round <click to place>

    change drill 3 <click via to change>

     

    If you want to attach the plated holes to a particular net you can use the 'name' command to change their net name.

     

    If you want the holes represented in the schematic which is a perfectly valid thing to do it'll probably take a minute or two to create library parts for the parts you require yourself.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rachaelp

    Thank you @rachaelp

     

    It really helped.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rachaelp

    Thank you @rachaelp

     

    It really helped.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rachaelp
    rachaelp over 10 years ago in reply to e14 Contributor

    You're welcome, glad I could help :-)