Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum ERC Error Different connections pin and pad.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 1522 views
  • Users 0 members are here
Related

ERC Error Different connections pin and pad.

marsheng
marsheng over 9 years ago

I've done a few boards before and all worked fine. Today I changed the pad sizes for a diode and put a small pad next to one pad for a direction pointer. 

When I updated all, all seemed ok, however the ERC gives Different connections on D1 pin and pad 2 (N$11 and N$18)

 

I haven't worked with N's before so I'm not sure what to do. N$11 connects a resistor to the diode. Not sure where N$18 is.

 

Along the same lines I have a warning POWER on IC1 VCC connected to N$20. it is correct but do I have to tell N$20 it is a power line ?

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 9 years ago

    Wallace Weideman wrote:

     

    I've done a few boards before and all worked fine. Today I changed the pad sizes for a diode and put a small pad next to one pad for a direction pointer.

    When I updated all, all seemed ok, however the ERC gives Different connections on D1 pin and pad 2 (N$11 and N$18)

     

    I haven't worked with N's before so I'm not sure what to do. N$11 connects a resistor to the diode. Not sure where N$18 is.

    Did you make the change in the schematic with the board closed? This is the usual culprit for consistency errors. You can show where your nets are in the schematic / board by doing: SHOW N$11 or SHOW N$18 from the command line. Then change the board and / or schematic until they match again.

     

    Wallace Weideman wrote:

     

    Along the same lines I have a warning POWER on IC1 VCC connected to N$20. it is correct but do I have to tell N$20 it is a power line ?

    No you don't need to do anything. It does the same when you have a power pin named for example VCC and you connect it to a global rail named say +5V, again it's correct but it'll whinge about that too. In the ERC you can select this error and click 'Approve' and then it won't whinge about it again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago

    Wallace Weideman wrote:

     

    I've done a few boards before and all worked fine. Today I changed the pad sizes for a diode and put a small pad next to one pad for a direction pointer.

    When I updated all, all seemed ok, however the ERC gives Different connections on D1 pin and pad 2 (N$11 and N$18)

     

    I haven't worked with N's before so I'm not sure what to do. N$11 connects a resistor to the diode. Not sure where N$18 is.

    Did you make the change in the schematic with the board closed? This is the usual culprit for consistency errors. You can show where your nets are in the schematic / board by doing: SHOW N$11 or SHOW N$18 from the command line. Then change the board and / or schematic until they match again.

     

    Wallace Weideman wrote:

     

    Along the same lines I have a warning POWER on IC1 VCC connected to N$20. it is correct but do I have to tell N$20 it is a power line ?

    No you don't need to do anything. It does the same when you have a power pin named for example VCC and you connect it to a global rail named say +5V, again it's correct but it'll whinge about that too. In the ERC you can select this error and click 'Approve' and then it won't whinge about it again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • marsheng
    marsheng over 9 years ago in reply to rachaelp

    I did have the board and schematic open. I closed the lot, deleted the diode and reinserted it and all came right.

     

    Whoa, the show is great, even does the board and this is great for checking power and earth lines.

     

    Is there a way to highlight unlaid tracks on the PCB? I know there is the thin white line but I missed one tiny line on the bottom of a board and I had already sent the file to the PCB co.

    ERC does not highlight this.