Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum PCB design hierarchy
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 551 views
  • Users 0 members are here
  • pcb board design
Related

PCB design hierarchy

perigalacticon
perigalacticon over 9 years ago

Looking for advice for designing a PCB with several functions.  I am an amateur PCB designer and only designed one other small board but it worked.

 

This project currently has the following features:

 

1.  5V & 3.3V power regulators.

2.  SPI signals from an ATTINY841-SU SOIC-14 MCU to a Dataflash SPI flash soic-8 IC.

3.  1W audio amplifier to external 8R .5W speaker.

4.  5x WS2812B surface mount Leds.

5.  5X capacitive touch pads (externally connected).

6 2x 6V  2CR1/3N2CR1/3N batteries in parallel

7.  2.25" square PCB, 2-sided, standard options.

 

I am looking for advice as to how to route the traces for best performance, I'm working with Eagle 8.3.2.  This a project for some gifts I am making for Halloween in a quantity of ~50.

 

I am mainly concerned about signal integrity, especially the capacitive touch connections.  Currently I routed these last but there are many vias on these traces and I'm concerned that nearby external objects may affect the capacitance readings.  I could route these first on top with no vias but then the other signal traces are more complicated.  Is SPI sensitive to routing with several vias?  How about WS2812B data signals or small voltage audio signals?  How sensitive should I expect this system to be to routing overall?  Are there recommended places to get advice?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    You've double posted this which is  a really bad idea - there are two replies in the other post.

    The other post (in Design Centre) has  a different title - so people won't realize at first that they are the same thing.

     

    Try to pick titles that describe the issue - how about "Looking for simple ATTiny pcb design advice"

     

    I suggest you delete this post.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 9 years ago

    You've double posted this which is  a really bad idea - there are two replies in the other post.

    The other post (in Design Centre) has  a different title - so people won't realize at first that they are the same thing.

     

    Try to pick titles that describe the issue - how about "Looking for simple ATTiny pcb design advice"

     

    I suggest you delete this post.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • perigalacticon
    perigalacticon over 9 years ago in reply to michaelkellett

    I would but I don't see an option to delete it.