Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 190 subscribers
  • Views 3970 views
  • Users 0 members are here
  • raspberry pi i2c
  • servo motor
  • i2c
  • how to i2c
  • pwm
  • raspberry pi io
  • servo
  • pwm controller
Related

needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller

tlucas756
tlucas756 over 8 years ago

So I saw a neat project on a magazine about controlling an rc-car wirelessly through a raspberry pi, using pwm.

I ordered everything I needed, mainly an i2c controller, and I started working on it. i am using a clone of the adafruit controller instead of a real one, because it was a lot cheaper, though the functionality remains the same.

Now, I have a problem. The article says that I need to connect the steering motor to the 3 pins on the adafruit controller, which are labeled power, ground, and PWM, but my motor only has two wires, so I have no idea what they do, or what to do next.

I do not have another rc-car to do this on. How do I connect the motor to the controller? do I need to get a different motor?

Thank you for your help!

image

imageimageimage

  • Sign in to reply
  • Cancel
Parents
  • ninjatrent
    ninjatrent over 8 years ago

    Hi Tiago,

     

    I have the Adafruit version of this part.

     

    I have also experienced taking a rc car apart to find this type of 6V motor for steering control. It is not as precise as a servo. If this is the only option for your project then I would recommend a L293D or L298N Dual H Bridge Motor driver. This will handle the 6V steering and drive motors on this car.

     

    This will be easier than replacing the steering motor with a servo.

     

    The 16 channel pwm/servo driver that you have purchased is a good part for a hexapod type robot or robotic arm. With this part you could include a servo controlled arm or a camera gimbal into your project. This pwm/servo driver might also be used to control RGB LEDs.It might also be possible to use this driver to control the esc on a quadcopter drone. Even if you can't use it with your current project, it might come in handy for a future project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ninjatrent
    ninjatrent over 8 years ago

    Hi Tiago,

     

    I have the Adafruit version of this part.

     

    I have also experienced taking a rc car apart to find this type of 6V motor for steering control. It is not as precise as a servo. If this is the only option for your project then I would recommend a L293D or L298N Dual H Bridge Motor driver. This will handle the 6V steering and drive motors on this car.

     

    This will be easier than replacing the steering motor with a servo.

     

    The 16 channel pwm/servo driver that you have purchased is a good part for a hexapod type robot or robotic arm. With this part you could include a servo controlled arm or a camera gimbal into your project. This pwm/servo driver might also be used to control RGB LEDs.It might also be possible to use this driver to control the esc on a quadcopter drone. Even if you can't use it with your current project, it might come in handy for a future project.