Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 190 subscribers
  • Views 3970 views
  • Users 0 members are here
  • raspberry pi i2c
  • servo motor
  • i2c
  • how to i2c
  • pwm
  • raspberry pi io
  • servo
  • pwm controller
Related

needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller

tlucas756
tlucas756 over 8 years ago

So I saw a neat project on a magazine about controlling an rc-car wirelessly through a raspberry pi, using pwm.

I ordered everything I needed, mainly an i2c controller, and I started working on it. i am using a clone of the adafruit controller instead of a real one, because it was a lot cheaper, though the functionality remains the same.

Now, I have a problem. The article says that I need to connect the steering motor to the 3 pins on the adafruit controller, which are labeled power, ground, and PWM, but my motor only has two wires, so I have no idea what they do, or what to do next.

I do not have another rc-car to do this on. How do I connect the motor to the controller? do I need to get a different motor?

Thank you for your help!

image

imageimageimage

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 8 years ago

    As Dave indicates a DC motor would need an H-Bridge to reverse polarity.

    The micro servo might work as a demo but may have problems in actual use. You need to check if the torque is enough, the speed is adequate, and the angle of rotation is sufficient.

    If all of that is okay, the wheels can typically transmit a high spike load to the motor when one wheel hits a bump or a wall. This will often strip the plastic gears in a servo motor. Servo-savers can reduce the spike load, but it may still need metal gears.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • tlucas756
    tlucas756 over 8 years ago in reply to dougw

    would this one work? it does have metal gears.

     

    YOURobot - Servo Motor Tower Pro MG995

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tlucas756
    tlucas756 over 8 years ago in reply to dougw

    would this one work? it does have metal gears.

     

    YOURobot - Servo Motor Tower Pro MG995

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dougw
    dougw over 8 years ago in reply to tlucas756

    The servo needs the rest of the internal circuitry to work like a servo. If you just use the motor, you will need the H-bridge just like any other DC motor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to tlucas756

    Ok - are you familiar with what's inside a servo motor though ?

     

    If not then you may want to take a quick look at this video:

    https://www.youtube.com/watch?v=9cvCRnVFpnA

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • tlucas756
    tlucas756 over 8 years ago in reply to beacon_dave

    I was planning on tearing the motor apart and only salvage the motor itself, because the assembly of the motor in the car already has the gears inside.

     

    Though, if I'm gonna do that, I'll just get the cheaper one, since I won't be using the metal gears

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to tlucas756

    Adafruit appear to approve of them:

    https://www.adafruit.com/product/1142

    "We now carry the Tower-Pro MG-995, they are very nice, high quality servos, excellent for use in robotics."

    The question is probably more a case of can you fit it into the car in place of the existing steer motor ?