Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum help with PCB layout checking
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 1483 views
  • Users 0 members are here
Related

help with PCB layout checking

houandreas
houandreas over 8 years ago

images uploaded.

hi, with your help I finally finished my first board in eagle. But I don't have any experience before, so there might be some mistakes to fix. Here I upload my board and schematic files in my google drive. If anyone could help me with this would be so appreciated.

https://drive.google.com/open?id=1Cm6o7Ets-rg0RCMyVHRzhi6eLX1H9t_D

This board is an adapter board for video signal processing. So it's running high frequcency signals I guess(pixel time 40ns). I read a lot about it but it's more than I can handle for now...

And the placement of those components is quite limited, that is already the best placement I can do. I used autorouter so there is no DRC error for now (I apply the default DRC setting).

here are some net settings for this board, you can also see it in eagle.

signal trace width 10mil, Via 15mil, clearance 10mil.

Power trace width 20mil, Via 20mil. clearance 10mil.

I cannot route if trace width is wider since the LPC connector pins are so close to each other. But this should be enough. Later I will make top and bottom as ground plane and add some via,but now is too late...Again thank you image

imageimageimage

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Bin,

     

    After using the autorouter, the DRC check still needs to be done, it cannot be assumed that it will do it for you (it doesn't as far as I understand, but I don't use the autorouter so Im not sure).

    If it passes DRC (and if you've already done the ERC on the schematic) then hopefully it should work to some extent, but it is really up to you to decide if it is adequate - there are many areas for improvement. For example, the power traces may need to be thicker (there is an automated way - assigning net classes - or you can manually change trace thickness) and power plane is helpful. For the latter, 'polygons are used in EAGLE. Also, many traces can be improved. For example, there could be signal buses, and the traces in those could be positioned next to each other, rather than what looks very random currently. It is ok to rip up traces and reattempt, or move some components if possible, to improve the trace paths.

    See here for an animated example of a real PCB, with several iterations:

    image

     

    If you are new to this, then as a suggestion maybe it is worth avoiding the autorouter for now, and manually trying to route it. It will take longer, but you'll learn more about how to use the functionality to place traces to your desired thickness and locations. Also a lot can be learned by looking at existing PCBs.

    I hope this helps.. prototype PCBs are cheap, so you can also learn by just trying it, if the DRC passes. If there are DRC failures then you need to try to understand each failure, since it takes just one to result in an unusable board.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Hi Bin,

     

    After using the autorouter, the DRC check still needs to be done, it cannot be assumed that it will do it for you (it doesn't as far as I understand, but I don't use the autorouter so Im not sure).

    If it passes DRC (and if you've already done the ERC on the schematic) then hopefully it should work to some extent, but it is really up to you to decide if it is adequate - there are many areas for improvement. For example, the power traces may need to be thicker (there is an automated way - assigning net classes - or you can manually change trace thickness) and power plane is helpful. For the latter, 'polygons are used in EAGLE. Also, many traces can be improved. For example, there could be signal buses, and the traces in those could be positioned next to each other, rather than what looks very random currently. It is ok to rip up traces and reattempt, or move some components if possible, to improve the trace paths.

    See here for an animated example of a real PCB, with several iterations:

    image

     

    If you are new to this, then as a suggestion maybe it is worth avoiding the autorouter for now, and manually trying to route it. It will take longer, but you'll learn more about how to use the functionality to place traces to your desired thickness and locations. Also a lot can be learned by looking at existing PCBs.

    I hope this helps.. prototype PCBs are cheap, so you can also learn by just trying it, if the DRC passes. If there are DRC failures then you need to try to understand each failure, since it takes just one to result in an unusable board.