Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Custom SMD in Eagle 9.1.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 190 subscribers
  • Views 4648 views
  • Users 0 members are here
  • smd
  • custom part
  • custom smd
Related

Custom SMD in Eagle 9.1.0

rgaillard
rgaillard over 8 years ago

I have been following these guides for making a custom smd layout:

 

https://www.autodesk.com/products/eagle/blog/what-you-didnt-know-about-eagle-arbitrary-pad-shapes/

 

https://www.youtube.com/watch?v=_G0ikZKB_Ss

 

And also these guides:

 

Library Basics Part 1: https://www.autodesk.com/products/eagle/blog/library-basics-part-1-creating-first-package-autodesk-eagle/

Library Basics Part 2: https://www.autodesk.com/products/eagle/blog/library-basics-part-2-creating-first-symbol-autodesk-eagle/

Library Basics Part 3: https://www.autodesk.com/products/eagle/blog/library-basics-part-3-creating-first-device-autodesk-eagle/

 

After following these guides I placed my part on a board. However I cannot route to the custom smd pads.  I repeated the process with unmodified smds, but I still can't route to the custom library part. Based on this, I'm guessed that whatever it is that I am doing wrong is covered in the Library Basics tutorials. However, I have started fresh twice following the tutorials but I still can't get it to work. I also followed the tutorials and made the same part as in the tutorials but I can't route to the tutorial part.

 

It looks like I am not allowed to attach the library file, so I will briefly describe what I did for my custom smd (omitting some details).

 

     First, I made the footprint by placing two smds on the top layer with the smallest default size from the size drop down menu. I renamed the smds with numbers 1 and 2. Now for the custom smd, I made two arcs in the top layer. Each arc completely covered 1 smd. The arcs do not overlap each other. I then made two more sets of arcs for tstop and tcream. Finally, I made name and value placeholders in the appropriate layers. From there I made the symbol and device making sure to connect the pins and pads.

 

I have attached an image of what the part looks like when placed it on a board (there are 2 parts in this image).

 

Thanks,

Randy

 

Message was edited by: Randy Gaillard

Attachments:
image
echo_electrode_arc_1mm_200um.zip
  • Sign in to reply
  • Cancel
  • rgaillard
    rgaillard over 8 years ago in reply to WarrenBrayshaw

    Wow! Thanks!

     

    I definitely want to avoid sparking. Sparking = bad

     

    The intended use is electroporation. I'll put a very small drop of fluid containing cells and plasmids in the center of the electrodes and give it a pulse. The electric field will cause the cells to open up allowing plasmids to get in. I'm planning on using a thick copper pour (probably 6 oz) with a silver or ENIG finish to get thick enough electrodes to generate a uniform field through the fluid. I'm playing around with different geometries to get the field i'm after, but I wanted to start working on the PCB footprint to make sure I don't design something that I can't make.

     

    You have been very helpful Warren. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenBrayshaw
    WarrenBrayshaw over 8 years ago in reply to rgaillard

    Hi Randy

     

    Your part is named "echo_electrode_arc_1mm_200um"

     

    If this is a spark gap and it's meant to have a 200um gap, it appears to have only a 100um gap

    Also a spark gap should not have solder stop in the gap so the footprint would need updating.

     

    I tried making the two arcs out of two arcs each and place the smd at the join. That worked out well and the part can exist on the board with no DRC errors.

    I've attached my effort but do check sizes etc. before you use it as it is a bit different to yours. The gap is 200um the circle is on the documentation layer. You can delete that.

    Inspect the package parts in the package editor of the library to understand whats been  done.

    Try it on a board and see how it behaves. - Enjoy

     

    Warren

    Attachments:
    echo_electrode_arc_1mm_200um2.zip
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenBrayshaw
    WarrenBrayshaw over 8 years ago in reply to rgaillard

    Hi Randy

     

    Your part is named "echo_electrode_arc_1mm_200um"

     

    If this is a spark gap and it's meant to have a 200um gap, it appears to have only a 100um gap

    Also a spark gap should not have solder stop in the gap so the footprint would need updating.

     

    I tried making the two arcs out of two arcs each and place the smd at the join. That worked out well and the part can exist on the board with no DRC errors.

    I've attached my effort but do check sizes etc. before you use it as it is a bit different to yours. The gap is 200um the circle is on the documentation layer. You can delete that.

    Inspect the package parts in the package editor of the library to understand whats been  done.

    Try it on a board and see how it behaves. - Enjoy

     

    Warren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rgaillard
    rgaillard over 8 years ago in reply to rachaelp

    What an annoying bug! I guess I should update to 9.1.1. Thanks for letting me know.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to rgaillard

    Hello,

     

    In 9.1.0 there is a bug which means the polygon button is missing in the footprint editor. I believe this has been fixed in 9.1.1. You can still create polygons by issuing the polygon command to the EAGLE command line in the footprint editor.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rgaillard
    rgaillard over 8 years ago in reply to WarrenBrayshaw

    Thanks for the reply. I did not realize that arc is treated differently than polygon. Actually, in 9.1.0 there is no polygon available when creating a footprint. The only available shapes are lines, circles, rectangles, and arcs. I've been assuming that all of these are considered as polygons.

     

    I have not tried autorouting, but I assumed it would potentially cause unwanted connections since I am able to do it manually when walk around obstacles is selected.

     

    I'll try and report back (maybe tomorrow) on what you have suggested about placing the pad at the end of an arc (or splitting the arc and placing it between the split arc). Though that may be more trouble than its worth at this point.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenBrayshaw
    WarrenBrayshaw over 8 years ago in reply to rgaillard

    HI

     

    You can create a board without a schematic but you do have to tell the board where the interconnections between pads are. You do this with the SIGNAL tool , on the board after ADDING the packages/elements /footprints. After that you can perform the routing.

     

    Turning off the thermals will likely not show any visual effects in your instance. I'm not sure but turning them off removes the possibility.

     

    The overlap errors are because you have not legitimately created the custom pads.  The smd needs to be on the end of a wire or surrounded by a polygon.

     

    The manual says the following for "Arbitrary pad shapes"

    "As soon as the center of the pad or SMD is inside the polygon's area or a wire begins at the center of a pad, it is recognized as a part of the PAD/SMD."

     

    You have used a wire (arc) so the smd needs to be at the end. Alas this is no good for your shape. I suspect you could split each arc and at the join of two arcs place the smd there.  Most simply you can just approve the overlap errors. The board will still be made correctly.

     

    tRestrict does not stop you manually routing over an area but the DRC check will show it. An autorouter is said to avoid the area.

     

    HTH
    Warren

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rgaillard
    rgaillard over 8 years ago in reply to WarrenBrayshaw

    Ok this helps a lot.

     

    Its been several years since I have made a PCB and even longer since I've made a custom pad. I didn't remember that I needed to create a schematic before I made a board. Making a schematic first allows me to route to the parts on the board.

     

    I unchecked thermals under properties for both pads. Does turning of the thermals for the smds in the footprint change anything visually? Why do you suggest turning them off?

     

    I'm still getting DRC overlap errors. Any idea how to fix that and if overlap errors would cause a problem if I wanted to have the board made?

     

    Also, I added a tRestrict arc to both pads hoping that would prevent routing through the pad. tStop is already there. As you can see in the image the N$2 trace is going through the pad for N$1. Is there anything I can do to prevent this?

     

    image

     

    Thanks for all the help everyone

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenBrayshaw
    WarrenBrayshaw over 8 years ago in reply to rgaillard

    Hi again

     

    On the schematic, when you move the device, do the nets stay attached?

     

    Hopefully you are using the NET tool to create the nets and not the WIRE tool. The WIRE tool will get you into trouble and while similar to the NET tool the NET tool has more features to assure you get nets connected to pins

     

    I'm using  Eagle 7.7 ,After I changed the grid of the symbol editor such that the pins were on the  0.1 inch grid, I had no problems creating a schematic, adding nets and seeing airwires on the board.

    So your library is fine. A point though; you may wish to turn off the thermal tick in the package as its not useful within your custom pads.

     

    Hope this helps

    Warren

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rgaillard
    rgaillard over 8 years ago in reply to rachaelp

    No I don't see any air wires and turning off walk around mode does not allow me to route to the part.

     

    I'm thinking that the problem must be with how I created the footprint but I'm at a loss as to where to start diagnosing the issue

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>