3M
  • Products & Partners
  • Manufacturers
  • 3M
  • More
  • Cancel
3M
Forum Signal Tracer (Old school)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3M to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 11 subscribers
  • Views 12866 views
  • Users 0 members are here
  • idea
Related

Signal Tracer (Old school)

supper_slash
supper_slash over 10 years ago

One of my projects for this year is to create a "new age" signal tracer like I used when i was a kid.

What I had was an old heathkit IT-12 pictured below.

image

 

The thing is i have no clue how this worked. I loved using it, and well just playing with it. It was sencitive efuff to hear audio runing through circuts without contacting the circuts, just getting the tip close to a trace.

 

So to start things off I created a audio amplifyer circut that I think is how this unit worked.

image

There are 2 things that I am compleetly lost about though.

 

  1. How to make, or what to use for the probe.
  2. How to make the visual circut.

1~I was thinking of taking a nail, and wraping copper wire around the nail to create a pickup coil, but i have no idea if this would work or if there is something better to try.

I am open to any ideas.

 

2~I was thinking of a 10 segment led bargraph desplay. But where would I need to conect the driver up to in the circut in the diagram? Would it be the the + side of C5?

I ordered some LM358N LM358 358 Low Power Dual Op-Amp IC's for this project that should be here on the 10th.

So I am planning on bread boarding this after that.

 

Also, I was thinking about starting to documenting some of my projects by video maby. So this might be one of the first ones I may try to document.

I have been feeling inspired by @Peter Oakes.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +2
    Great topic! Funnily enough, this is something I've been working on just a couple of days ago : ) The circuit I went for (not yet complete, but initial tests are ok-ish, I want to improve it) uses just…
  • shabaz
    shabaz over 10 years ago in reply to jc2048 +2
    Hi Jon, Exactly as you say, it would be good to build that into a small screened handheld enclosure (the FET part, if not the entire circuit), with a cable down to the battery box/speaker/LM386. Basically…
  • jw0752
    jw0752 over 10 years ago +1
    Hi Lupe, This sounds like a good project if you do any audio equipment servicing. I used to use a cheap imitation of the HeathKit in the old days. In your final design you are going to want a higher impedance…
Parents
  • shabaz
    shabaz over 10 years ago

    Great topic! Funnily enough, this is something I've been working on just a couple of days ago : )

    The circuit I went for (not yet complete, but initial tests are ok-ish, I want to improve it) uses just a single FET, the output is sufficient to drive headphones (or could append an audio amp to it, like LM386).


    As jw0752 says, you need a high input impedance, also the '358 circuit doesn't necessarily need the push/pull stage, it could probably drive a 64-ohm speaker with reasonable level of volume (64-ohm speakers are available from Farnell/Newark) or

    headphones with a lot of loudness. The push/pull stage as shown will have a lot of distortion but that's not an issue for such a test tool as you probably envisage the use of it (my circuit intentionally has excessive distortion for other reasons, depending

    on experiments I still want to do).

    Or use a LM386 for more output. An old Radio Shack test amplifier used the LM386 from memory too. The bar graph idea is very cool.

     

    For a TO-92 type device the  2N38192N3819 is an extremely popular JFET there are some example amplifier circuits here, about half-way down the page - I've not tried these though.

     

    As John says, the shielding will be super important otherwise there is a lot of hum.

     

    For the probe, a very expensive (but nice) option is a Pomona case - they have one which is aluminium and a useful size for a probe. I can try to dig out a part number if you require it. However I probably will go for a sweets/candy enclosure,

    something like a very small tin of mints for the high impedance input amplifier, and a cable to the rest of it (speaker/battery).

    For the pointy tip, filed steel could be used, but (again) Pomona sell a nice probe accessories kit that contains about five sharp tips, so good enough for 5 projects. It needs shielding though. So the coax idea from John is very good.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago

    Great topic! Funnily enough, this is something I've been working on just a couple of days ago : )

    The circuit I went for (not yet complete, but initial tests are ok-ish, I want to improve it) uses just a single FET, the output is sufficient to drive headphones (or could append an audio amp to it, like LM386).


    As jw0752 says, you need a high input impedance, also the '358 circuit doesn't necessarily need the push/pull stage, it could probably drive a 64-ohm speaker with reasonable level of volume (64-ohm speakers are available from Farnell/Newark) or

    headphones with a lot of loudness. The push/pull stage as shown will have a lot of distortion but that's not an issue for such a test tool as you probably envisage the use of it (my circuit intentionally has excessive distortion for other reasons, depending

    on experiments I still want to do).

    Or use a LM386 for more output. An old Radio Shack test amplifier used the LM386 from memory too. The bar graph idea is very cool.

     

    For a TO-92 type device the  2N38192N3819 is an extremely popular JFET there are some example amplifier circuits here, about half-way down the page - I've not tried these though.

     

    As John says, the shielding will be super important otherwise there is a lot of hum.

     

    For the probe, a very expensive (but nice) option is a Pomona case - they have one which is aluminium and a useful size for a probe. I can try to dig out a part number if you require it. However I probably will go for a sweets/candy enclosure,

    something like a very small tin of mints for the high impedance input amplifier, and a cable to the rest of it (speaker/battery).

    For the pointy tip, filed steel could be used, but (again) Pomona sell a nice probe accessories kit that contains about five sharp tips, so good enough for 5 projects. It needs shielding though. So the coax idea from John is very good.