3M
  • Products & Partners
  • Manufacturers
  • 3M
  • More
  • Cancel
3M
Forum Signal Tracer (Old school)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3M to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 11 subscribers
  • Views 12866 views
  • Users 0 members are here
  • idea
Related

Signal Tracer (Old school)

supper_slash
supper_slash over 10 years ago

One of my projects for this year is to create a "new age" signal tracer like I used when i was a kid.

What I had was an old heathkit IT-12 pictured below.

image

 

The thing is i have no clue how this worked. I loved using it, and well just playing with it. It was sencitive efuff to hear audio runing through circuts without contacting the circuts, just getting the tip close to a trace.

 

So to start things off I created a audio amplifyer circut that I think is how this unit worked.

image

There are 2 things that I am compleetly lost about though.

 

  1. How to make, or what to use for the probe.
  2. How to make the visual circut.

1~I was thinking of taking a nail, and wraping copper wire around the nail to create a pickup coil, but i have no idea if this would work or if there is something better to try.

I am open to any ideas.

 

2~I was thinking of a 10 segment led bargraph desplay. But where would I need to conect the driver up to in the circut in the diagram? Would it be the the + side of C5?

I ordered some LM358N LM358 358 Low Power Dual Op-Amp IC's for this project that should be here on the 10th.

So I am planning on bread boarding this after that.

 

Also, I was thinking about starting to documenting some of my projects by video maby. So this might be one of the first ones I may try to document.

I have been feeling inspired by @Peter Oakes.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +2
    Great topic! Funnily enough, this is something I've been working on just a couple of days ago : ) The circuit I went for (not yet complete, but initial tests are ok-ish, I want to improve it) uses just…
  • shabaz
    shabaz over 10 years ago in reply to jc2048 +2
    Hi Jon, Exactly as you say, it would be good to build that into a small screened handheld enclosure (the FET part, if not the entire circuit), with a cable down to the battery box/speaker/LM386. Basically…
  • jw0752
    jw0752 over 10 years ago +1
    Hi Lupe, This sounds like a good project if you do any audio equipment servicing. I used to use a cheap imitation of the HeathKit in the old days. In your final design you are going to want a higher impedance…
Parents
  • jw0752
    jw0752 over 10 years ago

    Hi Lupe,

         This sounds like a good project if you do any audio equipment servicing. I used to use a cheap imitation of the HeathKit in the old days. In your final design you are going to want a higher impedance input. The schematic you display has the resistance of the volume control as a load on your input. I think you will want a small capacitor in series with the input. If I was going to make a probe for one of these I think I would use a regular meter test probe and put a coax cable on it. At the probe I would expand the shielding over the handle of the probe and then cover it with heat shrink. This would keep interference down and give a good point with which to touch the circuit traces. With a capacitor in series you will not have to worry about touching a voltage rail. I have seen small bar displays that give a basic voltage level reading. You can drive the output of your amplifier into a voltage integrator and use the bar graph to read the voltage. You should be able to find some circuit suggestion if you google VU meter circuits. I look forward to seeing what you come up with.

     

         I use to see those indicator tubes, like the one on the Heath Kit, on some of the old radios that I used to play with. As the signal got stronger the green light of the display would close down. It was very cool.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 10 years ago

    Hi Lupe,

         This sounds like a good project if you do any audio equipment servicing. I used to use a cheap imitation of the HeathKit in the old days. In your final design you are going to want a higher impedance input. The schematic you display has the resistance of the volume control as a load on your input. I think you will want a small capacitor in series with the input. If I was going to make a probe for one of these I think I would use a regular meter test probe and put a coax cable on it. At the probe I would expand the shielding over the handle of the probe and then cover it with heat shrink. This would keep interference down and give a good point with which to touch the circuit traces. With a capacitor in series you will not have to worry about touching a voltage rail. I have seen small bar displays that give a basic voltage level reading. You can drive the output of your amplifier into a voltage integrator and use the bar graph to read the voltage. You should be able to find some circuit suggestion if you google VU meter circuits. I look forward to seeing what you come up with.

     

         I use to see those indicator tubes, like the one on the Heath Kit, on some of the old radios that I used to play with. As the signal got stronger the green light of the display would close down. It was very cool.

     

    John