Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Circuit Studio step file export fail
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 13 replies
  • Subscribers 95 subscribers
  • Views 3043 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Circuit Studio step file export fail

vadim007
vadim007 over 9 years ago

Hello!

I have some step file export fail.

image

I have never had this issue before. What should I do now?

  • Cancel

Top Replies

  • rfgeek
    rfgeek over 9 years ago in reply to cjmorcom +3
    Agreed, any error message would be helpful. I am fortunate to have access to Altium Designer to compare the two. The CS STEP exporter seems to have a number of issues that Altium Designer STEP exporter…
Parents
  • cjmorcom
    0 cjmorcom over 9 years ago

    Hi,

    We have the same issue:

    image

     

    For info:

    a) I have not imported the PCB edge from a dxf or any other file;

    b) the circuit board displays perfectly in 3D view mode; and

    c) other boards can be exported as step files without problem.

     

    Please can you help resolve this?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • cjmorcom
    0 cjmorcom over 9 years ago in reply to cjmorcom

    I traced the failure of the step export to a faulty 3D component body model that looked like this:

    image

    Replacing the model with one whose legs were attached to the component body cured the export problem.

     

    So, if step export fails, it's probably worth using the 3D view to zoom in close on all components and see that the 3D models are OK.

     

    Another way to find the problem component is to use the filter to select component groups and temporarily delete individual components (using a binary search approach makes it quicker), and then try the export until you have narrowed down which component(s) that are causing the problem. This is a bit tedious as you have to restart circuit studio after each failed export.

     

    It would be much better if Circuit Studio gave some meaningful error message: e.g. "Cannot export step - body of component U5 is incomplete"!

     

    Anyway, I hope this will be helpful to others.     

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • cjmorcom
    0 cjmorcom over 9 years ago in reply to cjmorcom

    I traced the failure of the step export to a faulty 3D component body model that looked like this:

    image

    Replacing the model with one whose legs were attached to the component body cured the export problem.

     

    So, if step export fails, it's probably worth using the 3D view to zoom in close on all components and see that the 3D models are OK.

     

    Another way to find the problem component is to use the filter to select component groups and temporarily delete individual components (using a binary search approach makes it quicker), and then try the export until you have narrowed down which component(s) that are causing the problem. This is a bit tedious as you have to restart circuit studio after each failed export.

     

    It would be much better if Circuit Studio gave some meaningful error message: e.g. "Cannot export step - body of component U5 is incomplete"!

     

    Anyway, I hope this will be helpful to others.     

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • rfgeek
    0 rfgeek over 9 years ago in reply to cjmorcom

    Agreed, any error message would be helpful.

     

    I am fortunate to have access to Altium Designer to compare the two. The CS STEP exporter seems to have a number of issues that Altium Designer STEP exporter does not.

     

    The Circuit Studio STEP exporter simply crashes. Take the same file imported to Altium Designer and it will export STEP file that renders fines.

     

    The CS STEP export also has issues with certain board outlines that contain arcs, sometimes they STEP file includes them, sometimes not, but again the same file exports correctly from Altium Designer.

     

    It would be nice if the developers could get this squared away.

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • yadhu22krish@gmail.com
    0 yadhu22krish@gmail.com over 9 years ago in reply to cjmorcom

    Hi john,

    I had the same problem...But i exported the same board into step using altium. There wasnt any problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • batuu
    0 batuu over 9 years ago in reply to rfgeek

    I can confirm this. I have a PCB with a shape made up of a rectangle and an semi circle arc. The step export completed without errors but the semicircle part was missing in the step file.

    Also some drill holes are not created correctly.

     

    Oliver