Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Rotate component in 1.4 is terrible HELP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 91 subscribers
  • Views 1850 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Rotate component in 1.4 is terrible HELP

ninjaninja
ninjaninja over 9 years ago

Hitting the spacebar while moving a component in the PCB editor used to rotate the component from 0 -> 90 -> 180 -> 270 -> 0.  This has been the way ECAD works since I got out of college.  This no longer works in circuit studio.  Spacebar during move shoots the component off screen ussually (heaven's knows where...  seems like it mirrors on the xy axis or something crazy).  Now I need to push into the component attributes and type in the new angle for EVERY COMPONENT in my layout...  This is terrible bug and requires some attention ASAP.

 

I realize this the "HotFix" thread, but this requires immediate attention.

 

This bug is making this product terrible in my opinion.  When will we see a fix for this?

 

Jerome

  • Cancel

Top Replies

  • ninjaninja
    ninjaninja over 9 years ago in reply to sun-boy +1 suggested
    Thanks Steve, I found that sometimes it works on a single component (like the first time you export you schematic to the PCB, and if you select the component through the "move" button on the ribbon), but…
  • rjcurtis
    rjcurtis over 9 years ago +1
    Been informed of a workaround via EEVBlog forum, use Shift + Space to rotate, no idea why, but it does seem to work.
Parents
  • e14softwareteam
    0 e14softwareteam over 9 years ago

    Escalating this to the developers.

     

    E14 Software Team

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • rjcurtis
    0 rjcurtis over 9 years ago in reply to e14softwareteam

    An update would be great, I needed to make a few tweaks to an existing board and have been hit by this.  I tried un-installing and re-installing CS but no difference.

     

    So need to go back to v1.3 to be able to have any chance of using CS, where can I get a download of that from?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • rjcurtis
    0 rjcurtis over 9 years ago in reply to e14softwareteam

    An update would be great, I needed to make a few tweaks to an existing board and have been hit by this.  I tried un-installing and re-installing CS but no difference.

     

    So need to go back to v1.3 to be able to have any chance of using CS, where can I get a download of that from?