Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum What font works best and where is the Default font selected?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 90 subscribers
  • Views 7151 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What font works best and where is the Default font selected?

jimku
jimku over 9 years ago

Is there a recommended font and preferred size (and minimum size) to use that will work best for the pcb silk-screening process to make it easy to see especially when debugging and troubleshooting? I read somewhere that the preferred font is Sans Serif with a 65 mil height for maximum legibility. When I open the properties for a Reference Designator, I see that I have the option of using TrueType or Stroke Font and for Stroke you must also choose a line Width. Selecting TrueType gives me the selection of using the TrueType fonts on my system but when select Stroke, I have a choice of Default, Sans Serif or Serif. Does anyone know where the Default is defined?

  • Cancel
Parents
  • tarribred61
    0 tarribred61 over 9 years ago

    Hello,

     

    That is an interesting question. I usually pick the stroke type Sans Serif since it is simple and the line dimensions (height and width) are actually close to the specified values.  I haven't figured out how the TrueType font sizes are determined in CS or Altium.

     

    I have found that whether it is legible or not will depend on how good the fabricator is.  I usually specify that silkscreen legend should be liquid photo imaged or direct legend printed for very small type. I have had some boards with legend as small as 30mil height and it is readable under magnification.  True screenprinted may be cheaper for larger and high volume designs. The ink tends to sag and blur though in my experience.

     

    If I end up with mixed methods (stroke vs. TrueType) in the design, for example because multiple people did some of the footprints, then I select all the text on the overlay layers using PCB Filter and change them to be consistent method and size with the PCB Inspector.  Then I can change them after that one by one for any that I want to be extra large and readable.  In Altium Designer it is easier to use Find Similar Objects to pick these objects but in CS you can use the filter selections through PCB Filter to get at them.

     

    If you get a PCB-Ruler from Digikey (https://www.digikey.com/product-detail/en/digi-key-electronics/PCB-RULER-12INCH/PCB-RULER-ND/5767550 ), you will see it has examples of arial and stroke fonts down to 0.5mm high.  To me, down to 0.8 or maybe 0.7mm is readable but with eye-strain.

     

    I guess my preferred size for text on the overlay is 1mm high (40mil) and 6 mil line width using stroke SansSerif when using 0402 size parts.  If the design is not as small, say 0805 scale, then 1.5mm (60mil) height legend is easier on the eyes.  If you are designing something for field service and especially for connectors that a user or test/production workers need to identify then make it as big and readable as possible.

     

    For the assembly layer, I typically prefer TrueType Arial of varying sizes for text.  I usually work with very small parts so I make an actual assembly layer with boxes close to courtyard size and put in the .Designator text string on the same Assembly Top layer in the symbol as a box outline.  If I take parts footprints from the vault I have to modify them to move the lines off the 3D Top layer to the Assembly Top.  If you do larger scale designs then maybe using the Overlay (silk) layers for assembly is OK.

     

    I don't know where the CS default is defined.  Maybe someone else can say.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tarribred61
    0 tarribred61 over 9 years ago

    Hello,

     

    That is an interesting question. I usually pick the stroke type Sans Serif since it is simple and the line dimensions (height and width) are actually close to the specified values.  I haven't figured out how the TrueType font sizes are determined in CS or Altium.

     

    I have found that whether it is legible or not will depend on how good the fabricator is.  I usually specify that silkscreen legend should be liquid photo imaged or direct legend printed for very small type. I have had some boards with legend as small as 30mil height and it is readable under magnification.  True screenprinted may be cheaper for larger and high volume designs. The ink tends to sag and blur though in my experience.

     

    If I end up with mixed methods (stroke vs. TrueType) in the design, for example because multiple people did some of the footprints, then I select all the text on the overlay layers using PCB Filter and change them to be consistent method and size with the PCB Inspector.  Then I can change them after that one by one for any that I want to be extra large and readable.  In Altium Designer it is easier to use Find Similar Objects to pick these objects but in CS you can use the filter selections through PCB Filter to get at them.

     

    If you get a PCB-Ruler from Digikey (https://www.digikey.com/product-detail/en/digi-key-electronics/PCB-RULER-12INCH/PCB-RULER-ND/5767550 ), you will see it has examples of arial and stroke fonts down to 0.5mm high.  To me, down to 0.8 or maybe 0.7mm is readable but with eye-strain.

     

    I guess my preferred size for text on the overlay is 1mm high (40mil) and 6 mil line width using stroke SansSerif when using 0402 size parts.  If the design is not as small, say 0805 scale, then 1.5mm (60mil) height legend is easier on the eyes.  If you are designing something for field service and especially for connectors that a user or test/production workers need to identify then make it as big and readable as possible.

     

    For the assembly layer, I typically prefer TrueType Arial of varying sizes for text.  I usually work with very small parts so I make an actual assembly layer with boxes close to courtyard size and put in the .Designator text string on the same Assembly Top layer in the symbol as a box outline.  If I take parts footprints from the vault I have to modify them to move the lines off the 3D Top layer to the Assembly Top.  If you do larger scale designs then maybe using the Overlay (silk) layers for assembly is OK.

     

    I don't know where the CS default is defined.  Maybe someone else can say.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • jimku
    0 jimku over 9 years ago in reply to tarribred61

    Thanks for reminding me about the digikey ruler that has the example text sizes and thicknesses. I don't have one but I borrowed one from a co-worker. For an experiment, I put a few samples of text on a layer then output the gerbers then finally using a gerber viewer with a measuring tool, I measured right on with the settings for a Sans Serif stroke font but only about 60% of the height specified for TrueType Arial.