Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Defining my own table in schematic capture
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 89 subscribers
  • Views 2902 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Defining my own table in schematic capture

chwast
chwast over 9 years ago

Hello,

 

I am sorry for maybe trivial question, but could you help me to find the answer where I can find a description how to define and include my own Table for the schematic? I can pull the templates but I would like to change several elements like company logo etc.. How I can do it?

 

Thank you in advance and sorry for a trouble.

 

With Best Regards,

  • Cancel
  • tarribred61
    0 tarribred61 over 9 years ago

    It is a good question.  Here is my suggestion.  The basic process I use is to make my own templates for whatever size and orientation I want and then save them.  When I want to start a new sheet I just copy the template and then open it up and begin.

     

    I suppose you could also save as a schematic template file which is a *.SchDot option in the save-as command.

     

    To make your own, open one of the existing templates that is closest to what you want. The default template is in the File >System preferences menu pop-up. Pick one that matches the size and orientation you want.  Then make a new schematic.

     

    If you don't like the default title block...right click on the background and choose options> sheet. Unselect the Show Template Graphics box.  On at least some of the templates that leaves just the border.  Or it might by the Title Block check box. It depends on the template. Now draw your own title box, add in text, etc.  For text you can use special strings that begin with the = character.  These change with the Document Options > Parameters tab.

     

    For your logo, just place in graphics.

     

    Do the same thing if you want to add in a revision block and maybe notes such as proprietary warnings.

     

    Save someplace as a schematic that you begin with.  Or you can save it as a template style and set as default for future use.

     

    I usually start a new sheet from a saved default schematic instead of a template because I put notes like PRELIMINARY or REVIEW COPY right on the page. I also put a default proprietary and confidential notice block that I want to edit as needed.  If I put those in the template I don't think I would be able to change them when they are promoted to the schematic.  Maybe there is a way but I do what works for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • chwast
    0 chwast over 9 years ago in reply to tarribred61

    Thomas.

     

    Thank you very much for quick and detailed information how to do it. I created my own table by re-using some of the templates. One last point which you can maybe you know is how to align the text inside the table so when I move the description how to move the area where I am inserting the text from Right Click - > Document Option -> Parameters ?

     

    Because what I observed is if I move the descriptions for example Date: ( Black font ) and then I typed the Time from Doc Options - Parameters ( Blue ) they are misaligned. How to prevent to happen maybe you know.

     

    Thank you very much in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 9 years ago in reply to chwast

    When you insert a text string (regardless of if it is using a special string such as from document parameters) you can view its properties (right click > properties) and choose the alignment and orientation.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • chwast
    0 chwast over 9 years ago in reply to e14softwareuk

    Peter,

     

    Thank you very much, however the problem is the following: When I open the template some of the information are available to edit but some of them like Title / Number / Revision Sheet not. When you fill the parameters in schematic they are automoatically filled the areas however I cannot edit the location in template

     

    image

     

    See above.

     

    My question is: How to make visible the filed after Number: in order to adjust the position in the frame?

     

    Thanks a lot

    Jacek

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 9 years ago in reply to chwast

    If I understand correctly you will need to edit the template and place a text string, e.g. add =Title to where you want the title text to appear.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    0 tarribred61 over 9 years ago in reply to e14softwareuk

    There is actually a library of title blocks.  You can open as a schematic library and add them to your sheet or modify and make new ones. I found mine in C:\Users\Public\Documents\Altium\CS\Templates with a file name of Schematic Title Blocks.SchLib.

     

    This may show you examples of how to set these up.  Once placed on the sheet you can move the text strings around.  You should be able to make similar revision blocks as desired for different sheet sizes.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • chwast
    0 chwast over 9 years ago in reply to tarribred61

    Thank you very much