Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Moving tab to new window is not working?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 93 subscribers
  • Views 2793 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Moving tab to new window is not working?

jaxxs
jaxxs over 8 years ago

Hello

 

First post here.

 

So I was once able to open a tab into a new window, have that window on another monitor and I could simple drag tabs from the main window to the new window.

I can no longer do this and I have to open each tab into it's own window. The drag icon suggests that it should be able but on release...nothing?

I'm not sure if it's due to a windows 10 Update as the current CS version was working but is no longer working?

 

Any help is much appreciated

 

Cheers,

Mark

  • Cancel

Top Replies

  • bugrobotics
    bugrobotics over 8 years ago in reply to e14softwareuk +1
    e14softwareuk wrote: Just to update everyone that it appears possible the latest Windows 10 version 1709 update may cause issues with CircuitStudio multi-monitor support but is still under investigation…
  • bugrobotics
    bugrobotics over 8 years ago in reply to e14softwareuk +1
    Ill preface my response by saying I know you have nothing to do with all of this, you're just doing your job and I mean no disrespect. Pointing to another developer who has the same issues is like saying…
Parents
  • jaxxs
    0 jaxxs over 7 years ago

    OK so in order for me to achieve what was once working, I now have to drag and drop the tab as quick as  I can. Any delay releasing the tab will fail.

    It works for me 100% of the time as long as I'm fast enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • diond31
    0 diond31 over 5 years ago in reply to jaxxs

    I've having the same exact problem.  CS was working great on Windows 7.  I recently upgraded to Windows 10, and now I'm also suffering with CS tabs not moving easily.  I can rearrange them, but I have to drag them several (2, 3, maybe 4) times quickly to get the tab to stick to its new position.  The very sad bit is; its been over TWO YEARS since the original post and nothing has been done to solve this problem by Altium (they seem to have the problem in their flagship AD product too).  ALTIUM - Solution Please!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • diond31
    0 diond31 over 5 years ago in reply to jaxxs

    I've having the same exact problem.  CS was working great on Windows 7.  I recently upgraded to Windows 10, and now I'm also suffering with CS tabs not moving easily.  I can rearrange them, but I have to drag them several (2, 3, maybe 4) times quickly to get the tab to stick to its new position.  The very sad bit is; its been over TWO YEARS since the original post and nothing has been done to solve this problem by Altium (they seem to have the problem in their flagship AD product too).  ALTIUM - Solution Please!!!