Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum New Schematic Library Designator and Comment not Visible
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 5 replies
  • Subscribers 91 subscribers
  • Views 3516 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

New Schematic Library Designator and Comment not Visible

jimku
jimku over 8 years ago

I'm having a problem creating a new schematic library. When I create a new schematic library, a component is automatically created called Component_1. The problem is that the Default Designator and Default Comment in the Properties paged are checked as visible but they are not visible in the symbol. I can add a parameter and check it as visible and it will show up visible in the symbol. If I add a component to this new library I get the same result in that the Default Designator and Default Comment in the Properties paged are checked as visible but they are not visible in the symbol. I have tried unchecking and saving and then checking but they still remain invisible. Is this a bug? How can I get the Designator and Comment to show up in new parts in a new library? If I create a new component in an existing library, the Default Designator and Comment show up checked and do show up visible in the symbol as expected. This problem only appears in newly created libraries.

  • Cancel

Top Replies

  • csiemer
    csiemer over 8 years ago in reply to jimku +1 verified
    Since Designators and comments are default to autoposition, their visibility in the Library can be disabled so you do not have to worry about their positions. Once placed into a schematic they will be…
  • jimku
    jimku over 8 years ago in reply to csiemer +1
    Thank you! I never had to change anything in the Library Editor Workspace for the comment and designator to show up before but I followed your instructions and now I see them. I don't know how it got un…
Parents
  • blackiyto
    0 blackiyto over 7 years ago

    Thank you!

    Lucky Patcher 9Apps VidMate

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • blackiyto
    0 blackiyto over 7 years ago

    Thank you!

    Lucky Patcher 9Apps VidMate