Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Silkscreen Cutout
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 10 replies
  • Answers 3 answers
  • Subscribers 90 subscribers
  • Views 5721 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Silkscreen Cutout

r.gibson
r.gibson over 8 years ago

I am building Capacitive Touch buttons for my project and am overlaying each button with silkscreen. At the center of each silkscreen area I want to cut out an icon to represent the buttons function (ie. a negative image). I am having trouble figuring out an efficient way to do this. I tried using a Polygon Pour Cutout on the Top Overlay layer, but it doesn't seem to work.

 

The best way I have figured out at this point is to draw a 360° arc, with a thickness of about 1/3 of the radius of the circle that it is filling (such that the outer radius of the arc is the same radius as the button) which leaves a 2/3 unfilled circle within. Then using filled rectangles, add to the silkscreen layer until the shape I want is formed. This is a huge PITA when all I really want are basic geometric shapes that would normally be easy to accomplish as a "positive" image (ie. make the shape out of Silkscreen instead of taking away silkscreen). Am I missing something?

  • Cancel

Top Replies

  • mars01
    mars01 over 8 years ago in reply to r.gibson +1 suggested
    Hi, Regarding your point 3. " 3) Select Tools -> Convert -> "Create Polygon From Selected Primitives" It has been discusses before. The command is not in the GUI but you can access it by typing "convert…
  • mars01
    mars01 over 8 years ago in reply to r.gibson +1 suggested
    You have them both, although you've asked for Create Polygon ... For Pour and Unpour, select and then right click on a Polygon, under the Polygon Actions selection there is a list with many possible actions…
  • mars01
    mars01 over 8 years ago in reply to r.gibson +1 suggested
    Yes, the search function is context sensitive. Welcome to the world of CircuitStudio: everything is but not quite.You have to dig through it, the search function is the same as it is on Altium Designer…
Parents
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    Polygon cutouts do work on the silk screen layer, you may need to right click on a polygon and Rebuild All to see the cutouts. Don't forget you can also have curved edges on polygons, just as when routing tracks use the SHIFT+SPACE to cycle through the available corner styles.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • r.gibson
    0 r.gibson over 8 years ago in reply to e14softwareuk

    Peter, thanks for the reply. I am using Altium Designer at work so I haven't had a chance to try your suggestion in Circuit Studio yet. I'll give it a try when I get home...in AD I'm having trouble finding the Rebuild All command. Is that a CS only function?

     

    Also, even in Designer I'm not able to subtract a simple geometric shape (triangle) from a circle. I'm using the Place->FullCircle function, which is not a polygon, so the Polygon Manager is not subtracting my Polygon Pour Cutout from it. How should I be creating a Polygon circle so I can then use the cutout?

     

    ...one more thing. Is it possible to rotate a polygon? For example, I have this circle with a triangle in it and I want to create alternate footprints with the triangle (arrow) pointing in various directions (D-pad). It would would be really convenient if I could just copy the footprint and then rotate the triangle, rather than having to redraw the triangle in each footprint. I tried selecting the polygon, then pressing the space-bar, which didn't work, and I don't see a rotate command anywhere else...Ahhhha, I just figured it out! You have to select and begin moving the polygon, THEN use the spacebar to rotate. Nevermind!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • r.gibson
    0 r.gibson over 8 years ago in reply to e14softwareuk

    Peter, thanks for the reply. I am using Altium Designer at work so I haven't had a chance to try your suggestion in Circuit Studio yet. I'll give it a try when I get home...in AD I'm having trouble finding the Rebuild All command. Is that a CS only function?

     

    Also, even in Designer I'm not able to subtract a simple geometric shape (triangle) from a circle. I'm using the Place->FullCircle function, which is not a polygon, so the Polygon Manager is not subtracting my Polygon Pour Cutout from it. How should I be creating a Polygon circle so I can then use the cutout?

     

    ...one more thing. Is it possible to rotate a polygon? For example, I have this circle with a triangle in it and I want to create alternate footprints with the triangle (arrow) pointing in various directions (D-pad). It would would be really convenient if I could just copy the footprint and then rotate the triangle, rather than having to redraw the triangle in each footprint. I tried selecting the polygon, then pressing the space-bar, which didn't work, and I don't see a rotate command anywhere else...Ahhhha, I just figured it out! You have to select and begin moving the polygon, THEN use the spacebar to rotate. Nevermind!