Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Generate Outputs not using entire page
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 13 replies
  • Subscribers 91 subscribers
  • Views 4757 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Generate Outputs not using entire page

adamwebber
adamwebber over 8 years ago

Something happened recently to my CS.  The PDF outputs are now filling a small portion of page.  I don't know what's going on.  I tried changing default prints scaling among other things.  It doesn't matter if it's an existing project or a new one.  Everything just changed somehow along the way.  Can anyone help?

Attachments:
image
image
image
image
  • Cancel
Parents
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    Hi James, assuming you are using Project | Generate outputs a few obvious things to check.

     

    For PCB Prints click Page Setup and check the scaling, paper size and corrections.

    image

    Might also be worth deleting (move or rename) your project's *.OutJob file and then re-define the print properties and re-generate the output. Another thought, have you installed any PDF printer driver software or similar recently?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • adamwebber
    0 adamwebber over 8 years ago in reply to e14softwareuk

    Yes, I am using Generate Outputs for the PDF creation.

    A Couple of things to note:

    1-The error has taken place since I installed a new Epson ET-3750 printer but I cannot be certain as to the exact time that the error began.  Whether it was before or after the printer was installed.

    2-I did have the size set up as Letter.  Changing it to A4 has made no difference. 

    3-Selecting 'Fit Document on Page' does not fix the problem. 

    4-Deleting the *.Outjob file and recreating it makes no difference.

    5-Starting a new project from scratch makes no difference.

     

    My next step is to completely remove CS and reinstall it.  I don't really want to do this since I like my current template and UI settings and I don't want to have to reconstruct or relocate them.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • adamwebber
    0 adamwebber over 8 years ago in reply to e14softwareuk

    Yes, I am using Generate Outputs for the PDF creation.

    A Couple of things to note:

    1-The error has taken place since I installed a new Epson ET-3750 printer but I cannot be certain as to the exact time that the error began.  Whether it was before or after the printer was installed.

    2-I did have the size set up as Letter.  Changing it to A4 has made no difference. 

    3-Selecting 'Fit Document on Page' does not fix the problem. 

    4-Deleting the *.Outjob file and recreating it makes no difference.

    5-Starting a new project from scratch makes no difference.

     

    My next step is to completely remove CS and reinstall it.  I don't really want to do this since I like my current template and UI settings and I don't want to have to reconstruct or relocate them.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to adamwebber

    I guess it is possible installing printer software has disturbed something. You could try a new installation to a different folder to save having to uninstall your current version, there is an option when installing to select a directory so just pick something a little different than the default. Another (rather random) idea is to check that your .Net framework hasn't been clobbered, see Error launching Layer Stack Manager  for some hints of repairing.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • csiemer
    0 csiemer over 8 years ago in reply to adamwebber

    This will be caused by a printer driver, I have seen it before as it used to happen rarely for Altium Designer as well, Epson drivers in particular seemed to be the most common.

     

    Sometimes you can correct it by reviewing the Page Size options for the printer driver or changing which printer is the Default within Windows.

     

    I have seen it corrected by installing a new generic print driver and setting that as default.

     

    If you uninstall the new printer, and then relaunch CircuitStudio you should be able to see if this corrected it.  If so, check to see if there are other drivers available for the printer that you can try, and also check the settings for that Printer within Windows to make sure the available page sizes are set properly.

     

    Reinstalling or modifying CircuitStudio likely will not help here.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • adamwebber
    0 adamwebber over 8 years ago in reply to csiemer

    Your advice is sound but I don't know how to fix this.  I first tried changing to another default printer with no improvement.  Then I uninstalled the driver with no improvement.  Then I restarted my computer with no improvement.  Then I installed a generic driver with no improvement.  I reinstalled the driver with no improvement.  I'm not sure what I need to do now.  Why does CS need to use the printer drivers?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to adamwebber

    It's quite possible that uninstalling the printer didn't undo everything. Do you have a system restore point just before installing the printer for the first time that you can roll back to?