Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Update a project with all component updates from multiple libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 90 subscribers
  • Views 2844 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Update a project with all component updates from multiple libraries

lamabrew
lamabrew over 8 years ago

A similar question was asked in the past (update a schematic with an updated library component, which is done by selecting the library component and the 'pushing' the update to the schematic, which must be open).  That is NOT the problem I need to solve.

 

I need to update every component in a project with the current symbol, parameters (for those that are linked), and footprint for every component in the project.  Opening every schematic sheet in the project and then going through every possible component in every possible library to make sure one doesn't get missed isn't workable.  I've searched through everything I can think of to figure out how to do this and I'm not finding the answer, apologies in advance if I missed the obvious.

 

Here's the use case I'm dealing with:

  • System with 6 PCB designs in it, each with multi-sheet schematics.
  • System specific (Altium Integrated) libraries, about a dozen (libraries for specific vendors, components, etc)
  • Working on PCB A, realize that half dozen library parts need modification (could be as simple updated supplier PN, or more serious like a footprint change)
  • Make the library mods and update PCB A to verify using the documented method to push changes from SchLib & PCBLib to schematics & layout for PCB A project
  • Now need to update schematics and layouts for PCB B, C, D, etc...

.

So far the only thing I can see is opening every schematic/layout in all of the PCB projects and then going back through each library with a written list of which components to push out an update to. IMHO the odds of getting every part in every project correct are zero; doesn't seem to be a way to run a report that would show where the project and the library have diverged?  There are definitely cases where I would not want to update a project with updated libraries - for example after release. But if you accidentally have a schematic page from something else open now that's been trashed if you push out the changes from the library side.

  • Cancel
Parents
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    It is possible to update all footprints from one library at a time.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jaza_tom
    0 jaza_tom over 8 years ago in reply to e14softwareuk

    I also am wondering how the heck to synchronize/update more than one component on my schematic at a time.

     

    I'm going through my schematic libraries and manually adding supplier links to each component.  Now that I have done that, I want the ability to either push all of those changes to my schematic document at the same time (from inside each library).  Alternatively, the ability to run a check from within my schematic document to see if any of the components in my design have corresponding source library diferences, and pull those differences to my schematic document.

     

    Thanks peterbarnard e14softwareuk

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to jaza_tom

    Sorry but I don't know of a way to mass update as you are looking to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jaza_tom
    0 jaza_tom over 8 years ago in reply to e14softwareuk

    Darn.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • jaza_tom
    0 jaza_tom over 8 years ago in reply to e14softwareuk

    Darn.