Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Compile warning for multiple net names...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 88 subscribers
  • Views 4206 views
  • Users 0 members are here
  • compile
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Compile warning for multiple net names...

tonyshell
tonyshell over 7 years ago

Hi,

 

  I compiled a schematic and I get a warning "Compiler Nets Wire +3.3VDC has multiple names (Power Object +3.3VDC,...Power Object GND).  It's saying that I named the same net with a different name.  So, I thought that, maybe I just copied and pasted and changed a 3.3 to a ground.  I tried deleting the offending nets and placed new ones in place of the old one, selecting power ground for the type of power.  That doesn't fix it!  What am I doing wrong?  Is this anything to worry about?  Thanks in advance.

  • Cancel
Parents
  • e14softwareuk
    0 e14softwareuk over 7 years ago

    Is this a multi-sheet design? Are you trying to connect power nets off-sheet yourself using ports rather than making use of the automatic power net naming feature set in Document Options : Options : Net Identifier Scope? If using default settings the power nets are global (using power net symbols) and do not need manually wiring up across sheets or hierarchy.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tonyshell
    0 tonyshell over 7 years ago in reply to e14softwareuk

    It is a multi-sheet design - flat, not hierarchical, only 3 sheets.  I'm just using the power port objects.  I'm not trying to connect them manually, I'm just placing a power port or copying and pasting an existing one.  See the picture for typical use.  Oh, great!  Another problem... now it won't even compile without getting an exception.  It still shows the warnings/errors, so maybe it's OK or I can do a recompile.  The Net Identifier Scope is still on the default setting - I haven't changed it.  Got any ideas?

     

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tonyshell
    0 tonyshell over 7 years ago in reply to e14softwareuk

    It is a multi-sheet design - flat, not hierarchical, only 3 sheets.  I'm just using the power port objects.  I'm not trying to connect them manually, I'm just placing a power port or copying and pasting an existing one.  See the picture for typical use.  Oh, great!  Another problem... now it won't even compile without getting an exception.  It still shows the warnings/errors, so maybe it's OK or I can do a recompile.  The Net Identifier Scope is still on the default setting - I haven't changed it.  Got any ideas?

     

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to tonyshell

    Hi Tony. A quick check - have you copied any online vault parts to create your own symbols? If not and you are still having problems then please feel free to send through the schematic and I will take a quick look on my system - software@element14.com.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tonyshell
    0 tonyshell over 7 years ago in reply to e14softwareuk

    Hi Peter, the only symbols I copied were the ones that used to create my own parts were the ones from the "Symbol" button on the Home ribbon bar.  What I'm getting warnings about are the power ports, actually that the wires connected to them.  For the GND power port, it named several dozen wires connected them "+3.3VDC".  How do I change the name of a wire?  Otherwise, I would have to delete and redo several dozen wires and it still might do the same thing.  Thanks in advance.

     

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tonyshell
    0 tonyshell over 7 years ago in reply to e14softwareuk

    Hi Peter, I just tried to delete a few wires and then redo them and it still names them as "+3.3VDC", at least that's what it highlights when I double-click the details from the warning message.  So, deleted the GND power port and all wires connected to it, then redid it.  When I recompiled, it gave me the same error and when I double-clicked "Wire +3.3VDC" in the details to highlight what wires were involved, it still highlighted the same wires, including the ones I just redid.  I don't know any way to even view what the net name of a wire is, so I'm assuming that it just named the new wires the same.

     

    I know this is just a warning, not an error, but I'm concerned that this will carry over the PCB part of the design and get the + and GND crossed.  Any help would be appreciated.

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to tonyshell

    Hi Tony. Not sure if you are saying you have copied power ports into your own parts. Normally these power ports are added directly to a design from the ribbon bar. The net name given in the property dialog for the power port is reflected in the name shown on the schematic and you should not need to name any net segment connected to such a port. If you have tried using the ports directly and still getting problems then please do consider sending through the design to software@element14.com for me to take a look at.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tonyshell
    0 tonyshell over 7 years ago in reply to e14softwareuk

    Hello Peter, sorry for the delayed response, I've had a few other things going on and have been very busy.  I'm not using ports in my parts, only in the schematics.  What I'm saying is that, when I get the compile warning and, when I click on the "Wire +3.3VDC" row in the details, it highlights all the GND ports as if they're connected to a +3.3VDC port... oh, never mind... I just did a double-check and found a +3.3VDC port shorted to a GND port!  It must have happened when I was moving a part (40-pin LCD connector) around.  It sometimes gets confused and puts junctions in if two wires get moved where they cross.  I compiled again and that warning went away.  I'll know the next time to look for that!  Thanks for your help.