Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum STEP file output won't include vias
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 6 replies
  • Subscribers 93 subscribers
  • Views 7465 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

STEP file output won't include vias

chuckbluz
chuckbluz over 8 years ago

I am trying to export a STEP file so my mechanical engineer can verify fit in the product housing. However the only vias and pads that are exported are those associated with a connector on the PCB. Even if I check all three selections in the Export Options menu, In other words the "Export Free Pad Holes" and "Export Mechanical Component Pad Holes" don't seem to work. This is critical, since some of these pads are used for alignment of the PCB into the housing during manufacture.

 

image

  • Cancel
Parents
  • DaveMcLaughlin
    0 DaveMcLaughlin over 8 years ago

    Older versions of Altium Designer had this bug and there is a chance the same code base is used for CircuitStudio. The latest Altium Designer 18 seems to have this fixed, at least so far none of the exported designs have any missing hole.

     

    What if you change to using a PAD instead of a VIA? Would that work?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • chuckbluz
    0 chuckbluz over 8 years ago in reply to DaveMcLaughlin

    I actually added some pads to use as reference holes, and that did not work either. I could live without the vias, but I don't see why the pads won;t show up.

     

    (the more I use CircuitStudio, the more I really dislike it)

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • lamabrew
    0 lamabrew over 8 years ago in reply to chuckbluz

    (using 1.5) I've only done the STEP output for a small PCB that plugs in to a larger PCB so I can't say how close this it to making the STEP usable in other tools, but my pads and (mounting) holes are in the STEP file.  (more obvious from the back, which doesn't have components). If it helps here's my example.

    image

     

     

    Here's my settings:

    image

    and a pad example:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • DaveMcLaughlin
    0 DaveMcLaughlin over 8 years ago in reply to chuckbluz

    Any chance you could include a sample of your board in step format? Export without the parts. Some 3D CAD software is better at handling this than others. My older Alibre Design didn't import holes but the same in Fusion 360 did.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • DaveMcLaughlin
    0 DaveMcLaughlin over 8 years ago in reply to chuckbluz

    Any chance you could include a sample of your board in step format? Export without the parts. Some 3D CAD software is better at handling this than others. My older Alibre Design didn't import holes but the same in Fusion 360 did.