Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum More bugs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 29 replies
  • Answers 1 answer
  • Subscribers 91 subscribers
  • Views 5511 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

More bugs

Sparkylabs
Sparkylabs over 7 years ago

1) If I go to edit my board shape I get put into some undefined mode where I cannot edit it or get out of it. The back button will undo things I have done whilst keeping me in a greyed out - out of control mode. The only way out is to close without saving and loose any changes not saved before entering the attempt to change board outline mode. I am also still confused as to why the outline needs defining twice! because unless I put a line around the board shape the autorouter gets confused and so does the PCB manufacturer! The board shape should define the outline in the Gerber. I can send an example project in.

 

2) Via's: I want to place a series of via's on my board. This board has several layers of different nets. I want my via's to be GND nets. I am constantly asked if I want to repour my plane, if I say yes this means that the plane has to be regenerated for every via I place and will take forever. if I say make unpoured then the via defaults to another net regardless of my setting. I guess I will have unpour all of my polygons and hope for the best! but really this all needs sorting out to make it easier. We have been through this before and demonstrated that things do not behave logically.

  • Cancel
Parents
  • Sparkylabs
    0 Sparkylabs over 7 years ago

    A further bug. If I have a polygon pour in a solder paste layer assigned to a net it also covers other nets in what will be a massive short circuit!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    0 voltsandjolts over 7 years ago in reply to Sparkylabs

    nonsense input = nonsense output

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Sparkylabs
    0 Sparkylabs over 7 years ago in reply to voltsandjolts

    You mean the options I am being given are a nonsense? If a net can be assigned it follows that only that net will be covered.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    0 voltsandjolts over 7 years ago in reply to Sparkylabs

    It appears that CS design rules are not applied to polygons on non-copper layers, they are not even assigned to a polygon class when on a non-copper layer. So, no, they won't work on the solder paste layer.

     

    However, it's very unusual to have large areas of solder paste that might be generated with polygons on the paste layer. If you are fixing a large (perhaps mechanical) component to the PCB by using a large area of solder paste there is a risk of shorting nearby nets due to the volume of solder which can be squeezed out during component placement. Normally you would use a sparse pattern of small paste squares to fix on larger areas.

     

    Paste mask is a whole science with some detail covered in IPC-7525 but this has a good introduction:

    http://www.jps-pcb.com/upfile/2017/02/20170216155446_850.pdf

    Page 27 illustrates my point but it's worth skim reading from page 10.

     

    If you say this is a bug in CS, I would say the bug is allowing polygons on the paste layers.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • voltsandjolts
    0 voltsandjolts over 7 years ago in reply to Sparkylabs

    It appears that CS design rules are not applied to polygons on non-copper layers, they are not even assigned to a polygon class when on a non-copper layer. So, no, they won't work on the solder paste layer.

     

    However, it's very unusual to have large areas of solder paste that might be generated with polygons on the paste layer. If you are fixing a large (perhaps mechanical) component to the PCB by using a large area of solder paste there is a risk of shorting nearby nets due to the volume of solder which can be squeezed out during component placement. Normally you would use a sparse pattern of small paste squares to fix on larger areas.

     

    Paste mask is a whole science with some detail covered in IPC-7525 but this has a good introduction:

    http://www.jps-pcb.com/upfile/2017/02/20170216155446_850.pdf

    Page 27 illustrates my point but it's worth skim reading from page 10.

     

    If you say this is a bug in CS, I would say the bug is allowing polygons on the paste layers.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • Sparkylabs
    0 Sparkylabs over 7 years ago in reply to voltsandjolts

    The polygon is a copy of a power polygon that has several TO-267 pakages on it with many via's, what little solder "all of that paste" actually translates into will likely go down the via's.