Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Disabling the snap function that should not exist
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 92 subscribers
  • Views 5291 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Disabling the snap function that should not exist

Sparkylabs
Sparkylabs over 7 years ago

That i can find there is no "snap" setting for the PCB layout environment. And yet trying to do any editing is more than the usual nightmare!!!! If I want to move something it is impossible to either "grip" it in the first place or it tries to force me to place things where i do not want them to go. To get a trace to move away from a collision I have caused by moving a component i hve to drag the trace in the opposite direction to the one it will flip in!!!! CRAZY.

 

Can I disable this pointless and time wasting behaviour? or is this another "missing feature" also known as a bug???

  • Cancel
Parents
  • adamwebber
    0 adamwebber over 7 years ago

    There is a snap function that you can change.  In the Home tab, there is an area called 'Grids and Units'.  Change your snap grid spacing here.  Select 'Properties' and you can adjust snap in the X and Y directions individually if you wish. 

     

    If you go to the File tab, select 'System Preferences' clear down at the bottom of the menu.  Under PCB Editor, select 'Interactive Routing'.  With this you can adjust the way that the PCB will route.

     

    Other than these two things, I don't know what else to say.  Other than it not being Altium, I rather enjoy using CS.  I can quickly turn out PCBs with no errors.  But I still prefer Altium.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Sparkylabs
    0 Sparkylabs over 7 years ago in reply to adamwebber

    Yes there is a grid setting but that has nothing to do with this. There are random snap conditions that jump several "snaps" of the grid. Trying to edit traces is a joke. As an example the "remove loops" does not work in trace edit and various strange entrails are left in editing. Yes it's not AD and based on this being a dumbed down version of AD I will never touch AD as clearly it is over priced.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    0 voltsandjolts over 7 years ago in reply to Sparkylabs

    Sounds like you might have "Snap to Object Hotspots" enabled.

    Home tab > Board Options > uncheck "Snap to Object Hotspots"

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • voltsandjolts
    0 voltsandjolts over 7 years ago in reply to Sparkylabs

    Sounds like you might have "Snap to Object Hotspots" enabled.

    Home tab > Board Options > uncheck "Snap to Object Hotspots"

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • Sparkylabs
    0 Sparkylabs over 7 years ago in reply to voltsandjolts

    THANK YOU! Yes indeed that might be the cause. Such a clever thing to have enabled by default. An option that stops you from moving a trace off a pad it has nothing to do with because the program wants to snap to the centre of the pad......... oh well, it is after all made in china.....

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • muessigb
    0 muessigb over 6 years ago in reply to Sparkylabs

    There is a minimum amount of competence required to use any PCB-EDA tool...

    Hotspot-snap is a common and useful feature that most PCB designers make use of.