Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum CS Keeps Having System/Running Errors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 11 replies
  • Subscribers 90 subscribers
  • Views 932 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

CS Keeps Having System/Running Errors

sclifford
sclifford over 7 years ago

I have now used CS latest version for two straight weeks.  Mind you I have been an Altium user now for years.  I must say I am very frustrated in getting this CS to operate properly.  It seems to be full of Bugs!

 

1st Problem

I keep getting system errors,  the last time to fix it I had to remove CS then reload it again.  This fixed the problem but then now another error appears.  When it does this its gets in some continuous loop of try to send the error message back to Altium.  This is so frustrating in trying to complete a simple board!

 

2nd Problem

I can not upload a standard DXF file into CS from Solid Edge.  What's with this, if I load the same file into Solid Works then load it back to CS it works.  This does not make any since at all, Is there a fix for this.  Currently I have to send my design files to a friend then he has to send them back to me so I can load them, this is such a pain!  I have noted this on the Community but no response.  In the past I have used Solid Edge files with AD and have had no issues at all.

 

3rd Problem

Why does CS not support a STP files to make board outlines.  I notice it was available in earlier versions, why was it removed?  CS/AD have such a good 3D environment why would you remove such a functional and needed feature?

 

Scott

  • Cancel
Parents
  • voltsandjolts
    0 voltsandjolts over 7 years ago

    Is there anything unusual about your system setup?

    For example, maybe you are working on a CS project that is stored in Dropbox?

    Or running in a virtual machine?

    I can't help but think there is something about the system which is triggering the problems you are seeing?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • sclifford
    0 sclifford over 7 years ago in reply to voltsandjolts

    No standard setup ... see this video i loaded up on YouTube

     

    https://youtu.be/OgAwmJl6YvM

     

    Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    0 voltsandjolts over 7 years ago in reply to sclifford

    Well, I've, never seen that bug either but I'm running 1.5.1 and never work with polys poured...poly pours are too sloooow and my patience quickly runs out, I just pour prior to design rule check.

    This is of no help, just saying that CS can work very well, guess I have luck on my side, so far!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • voltsandjolts
    0 voltsandjolts over 7 years ago in reply to sclifford

    Well, I've, never seen that bug either but I'm running 1.5.1 and never work with polys poured...poly pours are too sloooow and my patience quickly runs out, I just pour prior to design rule check.

    This is of no help, just saying that CS can work very well, guess I have luck on my side, so far!