Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum polygon region short circuit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 23 replies
  • Subscribers 88 subscribers
  • Views 7108 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

polygon region short circuit

acw210ee
acw210ee over 3 years ago

So i have polygons overlapping each other connected to nets, it seemed to draw them fine with J1 in the pcb however i get the DRC i get a short errors:

Clearance Constraint (Gap=6mil) (All),(All)
Polygon Region (93 hole(s)) Bottom Layer Pad J1-1(2129.921mil,-459.134mil) Multi-Layer
Polygon Region (88 hole(s)) Signal Layer 2 Pad J1-1(2129.921mil,-459.134mil) Multi-Layer
Polygon Region (93 hole(s)) Bottom Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (88 hole(s)) Signal Layer 2 Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (48 hole(s)) Top Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer


Back to top

Short-Circuit Constraint (Allowed=No) (All),(All)
Polygon Region (93 hole(s)) Bottom Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (88 hole(s)) Signal Layer 2 Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (48 hole(s)) Top Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer

When i remove J1 the problem goes away, however i am not sure what is causing it. As the issue with the polygon pours does not occur with the ot

her components. Should i just ignore the issue?

image

  • Cancel
Parents
  • GabeFromSpace
    GabeFromSpace over 3 years ago

    As Shabaz said, DRC errors should not be ignored unless the reason is known and acknowledged. Which layers of your PCB have polygons on them and which nets are they connected to?

    Having 2 overlapping polygons on the same layer with different nets is generally a "no no". If you have to have polygons on the same layer with different nets, they shouldn't be overlapping.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago in reply to GabeFromSpace

    Overlapping polygons is not a problem because when they are poured, they follow the design rules. My guess is that you need to repour the polygons.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago in reply to acw210ee

    Can you post a picture of J1 footprint?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GabeFromSpace
    GabeFromSpace over 3 years ago in reply to acw210ee

    Can you check out the footprint in your library editor? If you temporarily delete the 5 pads is there anything underneath? Also, can you screenshots of the polygon pour settings for each of your problem polygons?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • acw210ee
    acw210ee over 3 years ago in reply to GabeFromSpace

    i got the footprint from the altium vault FP-PJ-047A-MFGFP-PJ-047A-MFG

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GabeFromSpace
    GabeFromSpace over 3 years ago in reply to acw210ee

    The footprint looks pretty normal. When you double-click on the polygon, what does the Polygon Pour window look like?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to acw210ee

    At this stage you may as well start inspecting the Gerber files to see if the anomaly can be spotted.

    Could it be the thing shown below? The trace indicated with the orange arrow,seems to be on an inner layer. However, it is touching the light-grey shaded area indicated with the yellow arrow. 

    The light-grey area may be silkscreen perhaps, but if underneath that there is red pad, then that red pad copper will be on every inner layer. If this is the case it will be easy to see in the Gerber content. Or, perhaps you could switch off the silkscreen layers, to see where that red pad extends to. The component footprint isn't very good if the silkscreen is touching or overlapping the red pad. It should be a small distance away. It's not even needed to surround a through-hole pad, I don't see the point of that.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • acw210ee
    acw210ee over 3 years ago in reply to acw210ee

     image

    I think this might be an error with circuit studio. As when i move the copper plane away like this the drc errors go away (you can see the polygons are still overlapping on other parts of the pcb and i get no DRC error). However when i move that copper polygon (which is connected to ground) back over J1 the errors come back for pin 3 (no connect) and pin 1 (12V).

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GabeFromSpace
    GabeFromSpace over 3 years ago in reply to shabaz

    The trace indicated by the orange arrow is on a mechanical layer and shouldn't interact with the Short circuit part of the DRC. It's meant for the design stage and shouldn't show up in the gerbers. the light gray area is a multi-layer pad, meaning it's a pad on the top, inner, and bottom layers. The red pad is a *hopefully plated slot. The silkscreen is the lighted traces on the footprint. That being said, exporting a gerber file and opening it up in a separate viewer like Gerbview would be a good idea at this point.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago in reply to shabaz

    The DRC errors points to pads 1 & 3, apparently the GND polygon is touching those pads.

    acw210ee try closing CS, opening again, repour all the polygons, run DRC again.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • acw210ee
    acw210ee over 3 years ago in reply to shabaz

    i looked at those traces and those are on the "top overlay" in the pcb footprint. whats interesting is i get no error for pin 5 when i do the drc only pins 1 and 3

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GabeFromSpace
    GabeFromSpace over 3 years ago in reply to charlieo21

    ^ I second this.

    I've also had a buggy install of CS before. If the gerber files look good, and all else fails, it might not hurt to uninstall and reinstall it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • GabeFromSpace
    GabeFromSpace over 3 years ago in reply to charlieo21

    ^ I second this.

    I've also had a buggy install of CS before. If the gerber files look good, and all else fails, it might not hurt to uninstall and reinstall it.