Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Variant Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 11 replies
  • Subscribers 90 subscribers
  • Views 3839 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Variant Issues

adamwebber
adamwebber over 9 years ago

I am working with variants in CS.  I have declared the variant options to show the RED X on the schematics when parts are not fitted.  However, when I select the variant with not fitted parts, only the PCB is affected.  The schematics do not change.  How do I set it up so that it shows not fitted parts on both the schematic and PCB?  Rather, how do I display the RED X for not fitted components on the schematics?

 

My current steps:

1-Open Variant Manager

2-Add Variant

3-Name the Variant

4-Click OK

5-Select components "Not Fitted" in variant

6-Make sure that the variant options are selected in the schematic and PCB.

7-In Project Actions, select variant from drop-down menu. 

8-Watch as the schematic does not change.

9-Watch as the PCB changes by making components disappear.

 

This is also the case when generating outputs.  I can only generate the No Variant output of the schematics.  The PCB works though.

Attachments:
image
image
image
  • Cancel

Top Replies

  • harvie256
    harvie256 over 9 years ago in reply to e14softwareteam +1
    So the answer the question I asked... No Circuitstudio does not support multi-channel Variants like Altium Designer has for the last few generations. That's a shame, I use hierarchical multi-channel schematics…
  • vaidasmm
    vaidasmm over 9 years ago in reply to jamesharrimanaltium +1
    Thank You very much, now it works just fine .
Parents
  • e14softwareteam
    e14softwareteam over 9 years ago

    From the developers:

     

    Home > Project > Compile will compile the schematic and add the Compiler Tab at the bottom left of the schematic, adjacent to the Editor tab. Click the Compiler tab and the Not Fitted components will display the red X (provided the Drawing Style hasn't been changed to not show it) over the component.

    When Generating Outputs, for Schematic Prints you must click the Configure link and change from Logical Documents to Physical Documents. This is so that the software doesn't just print out the schematics as they were edited, but rather the compiled version for the Variant you're saving to PDF.

    Think of Physical as what will be physically present on the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • harvie256
    harvie256 over 9 years ago in reply to e14softwareteam

    Could you tell us which version of Altium Designer the Variants feature is based off?  They are discussed here: Multi-Channel Support for Variants | Online Documentation for Altium Products

     

    I used it on a recent design involving a multi-channel schematic (it's actually open source, you can see it here https://forum.makehackvoid.com/t/open-hardware-multi-meter-scanner-card/1024 )

     

    However, once I place the schematic sheet symbol on the top level schematic and used the Repeat command, all the components tagged to the variant disappeared from the variant manager.  What it's been replaced with is a separate  component for every channel of the design without the Not Fitted aspects in each variant (hopefully that made sense!)

     

    Does this mean it's actually the very early version of Altium's "Variants" that is incompatible with multi-channel designs?  Or am I doing something wrong?

     

    For example all the R7's and R9's should be Not Fitted in the capture below.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • harvie256
    harvie256 over 9 years ago in reply to e14softwareteam

    Could you tell us which version of Altium Designer the Variants feature is based off?  They are discussed here: Multi-Channel Support for Variants | Online Documentation for Altium Products

     

    I used it on a recent design involving a multi-channel schematic (it's actually open source, you can see it here https://forum.makehackvoid.com/t/open-hardware-multi-meter-scanner-card/1024 )

     

    However, once I place the schematic sheet symbol on the top level schematic and used the Repeat command, all the components tagged to the variant disappeared from the variant manager.  What it's been replaced with is a separate  component for every channel of the design without the Not Fitted aspects in each variant (hopefully that made sense!)

     

    Does this mean it's actually the very early version of Altium's "Variants" that is incompatible with multi-channel designs?  Or am I doing something wrong?

     

    For example all the R7's and R9's should be Not Fitted in the capture below.