Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Generate Outputs stuck in grayscale
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 18 replies
  • Subscribers 90 subscribers
  • Views 3342 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Generate Outputs stuck in grayscale

spe672
spe672 over 9 years ago

I can't get the batch job generate outputs function to allow me to make a color PDF of the schematic.  I have found where I can make the schematic mono, color and grayscale for individual prints, but I don't have the full version of acrobat...so it seems the only way to make a PDF is through the batch job where the schematic is stuck in grayscale.

 

Here's where I can batch output the schematic, but no color options seem to be available.

image

 

The options I get when I "Configure" the schematic print.

image

 

This panel affects individual prints, but I don't want a hard copy.  I need the batch to follow the color setting I've set here...

image

 

Thanks!

Andy

  • Cancel

Top Replies

  • harvie256
    harvie256 over 9 years ago in reply to spe672 +1
    Like wise I used AD professionally, but now that I run a small business, when I get grumpy about using the cut down version I just think about the amount of money that hasn't left my wallet!
  • harvie256
    harvie256 over 9 years ago in reply to jstrautman +1
    You are much better off just hacking the OutJob file, when you print to a PDF you're rending a image then compressing it. The file size ends up much bigger (like 20x) and you loose the great capability…
Parents
  • jstrautman
    jstrautman over 9 years ago

    Any chance you can use a pdf printer like "cutepdfprinter" or something similar to make the color prints you need?

     

    That's what I have been doing when I need to provide a color print to make it look more professional.  I do like the look of a color print much better than the greyscale.  The thing you lose is the ability to select components and nets in the bookmark section.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • harvie256
    harvie256 over 9 years ago in reply to jstrautman

    You are much better off just hacking the OutJob file, when you print to a PDF you're rending a image then compressing it.  The file size ends up much bigger (like 20x) and you loose the great capability of auto generating a complete and bookmarked document stack.

     

    All you have to do is open the <project name>.OutJob in your favourite text editor and do a search and replace for "PrintKind=1" to "PrintKind=0". Save it and you're now generating colour docs.

     

    I wrote a powershell script to do this, but since you only have to do it once per project I've never found it really any quicker than using a notepad++

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to harvie256

    At work, I developed our Altium templates;  we have an .outjob that travels with each project as a template file and the CS outjob doesn't exactly have this capability.  We start each PCB with a prjpcb, PCBdoc, several SCHdocs and outjob.  The outjob has been tailored to contain 4 output containers towards our release process; 2 for PCB release and 2 for assembly release.  It's a one stop shop outjob for our company and since we've got 50+ people using our floating seats, we have to simplify where we can for drawing release consistency.

     

    I opened the CS outjob file to try and tweak it so I could keep the project out settings common to my typical jobs, but got lost in all the stuff in there.  I'm specifically talking about setting up an outjob for  Schematic generation appended to a  specific PCB view (specific layers and with some draft view settings to make some stuff clear) and then gerber layers.  I would set up templates for a 2, 4 and 6 layer boards.  I messed with this during the first board I was working on in December.  I've since resorted to setting up each outjob on it's own (on my 4th board now) and it's not so bad, but I know i'm going to miss a detail on one of these jobs...

     

    My question is, what's your outjob workflow in CS since you're familiar with the power of output containers?  Have you found a good way to make a "Template" outjob?  I made one, but it retained some details of the original project it was associated with.  When it made the outputs folder, it kept the name of the original project, etc and didn't do what I was hoping it would.  I guess I could dig around till I made it work the way I wanted to, but haven't been motivated to attack that yet.

     

    Thanks

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • harvie256
    harvie256 over 9 years ago in reply to spe672

    I haven't got anything thoroughly worked yet, but the most promising thing from my perspective is to setup a template outjob then use simple powershell (or whatever floats your boat) scripts to replace the text elements necessary for each new project.

     

    So far the only way I've found to work with CS outjobs is a combination of setting stuff up roughly how I want it in the dialogs then modifying the outjob file to finish it off.  There's just too much missing from the CS outjob dialogs.  Also the outjob file is very easy to modify since it's all human readable text.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to harvie256

    I was scared of messing with the text in there, but running two simple find and replace functions in Notepad++ does exactly what I need!  Thanks for pointing me in the right direction, you killed two birds with one stone!  I had to tweak both the outjob and the prjpcb file to make it work. 

     

    I know extremely little about scripting, but I have several coworkers that can fix me up.

     

    thanks!

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jamesharrimanaltium
    jamesharrimanaltium over 9 years ago in reply to spe672

    Page Setup dialogs are being added to CircuitStudio in the up coming version 1.4. In the mean time it's no problem for you to hack the OutJob file carefully as described by harvie256 as this won't conflict with the up coming feature.

     

    Best regards,

    James Harriman

    Altium

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to jamesharrimanaltium

    I'm glad to see this will be improved, thank you for monitoring the pulse of this community and responding in a positive manner. 

     

    An similar question I've come up with is since learning to edit these tiles; is it possible to tweak gerber out file extensions?  I've not found where this can be modified in the text files.  One of the board houses I use (OSHPark) requires the outline layer to be  called *.GKO and CS outputs a *.outline file by default.  I can edit them after the files are generated if it's a fixed naming convention.

     

    Thanks!

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jamesharrimanaltium
    jamesharrimanaltium over 9 years ago in reply to spe672

    Hi Andy,

     

    No problem! It's good to see CircuitStudio popularity gaining ground with enthusiastic users!

     

    There is no control over the Gerber file names, so even if you rename the TopLayer to xLayer, the gerber plot for that layer will be named *.GTL.

     

    Best regards,

    James Harriman

    Altium

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to jamesharrimanaltium

    Thanks for the reply!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jstrautman
    jstrautman over 9 years ago in reply to jamesharrimanaltium

    James, do you have a rough idea of when this new 1.4 version of CS will be released?  And some quick big changes that will be made?  Thanks!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jamesharrimanaltium
    jamesharrimanaltium over 9 years ago in reply to jstrautman

    Hi jstrautman and Andy,

     

    Yes the 1.4 version is in Beta and assuming all goes well it should be only a few weeks away!

     

    The most amount of changes are related to the already excellent EAGLE importer, which will be getting even more features/improvements in CircuitStudio 1.4.

     

    Along with some other bug fixes we're also adding some minor features such as the Net Class Directive to Schematic so you can specify a Net Class on power nets for example, and update them to the board. In PCB we're therefore adding a Classes dialog so that you can edit/view the Net Classes, and added Net Class support to the appropriate rules.

    And as I mentioned earlier we added Page Setup options to Generate outputs files allowing, for example, color PDF outputs, but also other page setup settings you may want to change.

     

    Inclusion of these features are subject to Beta testing, of course.

     

    Best regards,

     

    James Harriman

    Altium

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to jamesharrimanaltium

    Thanks for the update, can't wait to see it!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • spe672
    spe672 over 9 years ago in reply to jamesharrimanaltium

    Thanks for the update, can't wait to see it!