Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Generate Outputs stuck in grayscale
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 18 replies
  • Subscribers 90 subscribers
  • Views 3342 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Generate Outputs stuck in grayscale

spe672
spe672 over 9 years ago

I can't get the batch job generate outputs function to allow me to make a color PDF of the schematic.  I have found where I can make the schematic mono, color and grayscale for individual prints, but I don't have the full version of acrobat...so it seems the only way to make a PDF is through the batch job where the schematic is stuck in grayscale.

 

Here's where I can batch output the schematic, but no color options seem to be available.

image

 

The options I get when I "Configure" the schematic print.

image

 

This panel affects individual prints, but I don't want a hard copy.  I need the batch to follow the color setting I've set here...

image

 

Thanks!

Andy

  • Cancel

Top Replies

  • harvie256
    harvie256 over 9 years ago in reply to spe672 +1
    Like wise I used AD professionally, but now that I run a small business, when I get grumpy about using the cut down version I just think about the amount of money that hasn't left my wallet!
  • harvie256
    harvie256 over 9 years ago in reply to jstrautman +1
    You are much better off just hacking the OutJob file, when you print to a PDF you're rending a image then compressing it. The file size ends up much bigger (like 20x) and you loose the great capability…
  • spe672
    spe672 over 9 years ago in reply to jamesharrimanaltium

    I'm glad to see this will be improved, thank you for monitoring the pulse of this community and responding in a positive manner. 

     

    An similar question I've come up with is since learning to edit these tiles; is it possible to tweak gerber out file extensions?  I've not found where this can be modified in the text files.  One of the board houses I use (OSHPark) requires the outline layer to be  called *.GKO and CS outputs a *.outline file by default.  I can edit them after the files are generated if it's a fixed naming convention.

     

    Thanks!

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jamesharrimanaltium
    jamesharrimanaltium over 9 years ago in reply to spe672

    Hi Andy,

     

    No problem! It's good to see CircuitStudio popularity gaining ground with enthusiastic users!

     

    There is no control over the Gerber file names, so even if you rename the TopLayer to xLayer, the gerber plot for that layer will be named *.GTL.

     

    Best regards,

    James Harriman

    Altium

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to jamesharrimanaltium

    Thanks for the reply!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jstrautman
    jstrautman over 9 years ago in reply to jamesharrimanaltium

    James, do you have a rough idea of when this new 1.4 version of CS will be released?  And some quick big changes that will be made?  Thanks!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jamesharrimanaltium
    jamesharrimanaltium over 9 years ago in reply to jstrautman

    Hi jstrautman and Andy,

     

    Yes the 1.4 version is in Beta and assuming all goes well it should be only a few weeks away!

     

    The most amount of changes are related to the already excellent EAGLE importer, which will be getting even more features/improvements in CircuitStudio 1.4.

     

    Along with some other bug fixes we're also adding some minor features such as the Net Class Directive to Schematic so you can specify a Net Class on power nets for example, and update them to the board. In PCB we're therefore adding a Classes dialog so that you can edit/view the Net Classes, and added Net Class support to the appropriate rules.

    And as I mentioned earlier we added Page Setup options to Generate outputs files allowing, for example, color PDF outputs, but also other page setup settings you may want to change.

     

    Inclusion of these features are subject to Beta testing, of course.

     

    Best regards,

     

    James Harriman

    Altium

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to jamesharrimanaltium

    Thanks for the update, can't wait to see it!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jstrautman
    jstrautman over 9 years ago in reply to jamesharrimanaltium

    Yes, very much appreciate the update.  Perhaps someone here should start a thread where people can suggest and discuss features to be added in future updates as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jamesharrimanaltium
    jamesharrimanaltium over 9 years ago in reply to jstrautman

    No problem, spec672 and jstrautman!

     

    We'll keep a look out on these threads for the suggestions.

     

    Best regards,

     

    James Harriman

    Altium

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
<