Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum CircuitStudio - Generate output files
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 5 replies
  • Subscribers 91 subscribers
  • Views 1741 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

CircuitStudio - Generate output files

michael_n
michael_n over 9 years ago

How can I export 1 output file only? Every time when I select for example the BOM only and click on Generate, CS still export all kind of file like SCH, Gerber, NC Drill, PnP, Documentation....

Attachments:
image
  • Cancel

Top Replies

  • adamwebber
    adamwebber over 9 years ago +2
    The export feature for CS is absolutely horrible. Altium is soooooo much better. I find myself frustrated in most cases when I try to export files. So instead of using the check boxes on the export feature…
  • michael_n
    michael_n over 9 years ago in reply to adamwebber +1
    The more time I spend with CS, the more i miss AD
  • michael_n
    michael_n over 9 years ago +1
    I'd try to modify the Assembly Drawings-> Configure -> ok to add/remove layer "Mechanical 1" but can't add/remove "Mechanical 13" or "Mechanical 15" Just wonder how many programmer/tester are working on…
Parents
  • adamwebber
    adamwebber over 9 years ago

    The export feature for CS is absolutely horrible.  Altium is soooooo much better.  I find myself frustrated in most cases when I try to export files.  So instead of using the check boxes on the export feature, I create an *.OutJob file and edit that.  For example, I like to have both top and bottom sides of the board as 3D print but the export window only allows either the Top or the Bottom but not both.  So I create an export for the Top and save the *.OutJob file then I create an export for the bottom.  Then I merge both files into one using a text editor like Notepad++ and list them sequentially.  In the *.OutJob file there is a line for each output type called OutputEnabledX=Y where X is the number of the output and Y is 0 (False) or 1 (True).  So when I want to generate the output, instead of clicking on a checkbox in the export window, I edit the text file instead and then click "Generate".  It's a little cumbersome but that's the price you have to pay when you pay $1000 for CS instead of $8000 for Altium.  $1000 is still a lot.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • n.wrightson
    n.wrightson over 9 years ago in reply to adamwebber

    Hi James,

    I understand what you are doing but where are you performing these actions from?

    What is the export button that you are using to generate the *.OutJob?

    Then how are you executing the OutJob?

    Neil.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • adamwebber
    adamwebber over 9 years ago in reply to n.wrightson

    Under the HOME tab, select the PROJECT drop down.  Select GENERATE OUTPUTS.  This brings up a window with all of the available exports.  Check any number of boxes and click the GENERATE button.  This will create your *.OutJob file.  Once this has been created, you can edit the file with any text editor.  I recommend making a copy of the original before messing around with this because CS is really stupid when it comes to looking at files edited outside of CS.  Mess around with this a lot.  Spend half a day testing out exports and see what you can change.  It's really pathetic and I miss the file generation of Altium.  But this is my best workaround.  I recommend making a small test project as it will be easier to find what you are looking for.  Good Luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • adamwebber
    adamwebber over 9 years ago in reply to n.wrightson

    Under the HOME tab, select the PROJECT drop down.  Select GENERATE OUTPUTS.  This brings up a window with all of the available exports.  Check any number of boxes and click the GENERATE button.  This will create your *.OutJob file.  Once this has been created, you can edit the file with any text editor.  I recommend making a copy of the original before messing around with this because CS is really stupid when it comes to looking at files edited outside of CS.  Mess around with this a lot.  Spend half a day testing out exports and see what you can change.  It's really pathetic and I miss the file generation of Altium.  But this is my best workaround.  I recommend making a small test project as it will be easier to find what you are looking for.  Good Luck.