Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum All I want is a resistor....
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 26 replies
  • Subscribers 97 subscribers
  • Views 9809 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

All I want is a resistor....

Sparkylabs
Sparkylabs over 9 years ago

I am a bit baffled by the total lack of basics. I can install all sorts of manufacturer specific libraries but if I want a resistor, or capacitor of other generic part I need to create it from scratch ? As CS is supplied by Farnell why is there not a basic library of what they supply available ?

 

The whole library part of CS seems to be a joke, and no I have no interest in the vault, it is impossible to search very hard and slow to use and not available if I am off line. Many parts are missing from the vault, there is a multicomp section (yes farnells own brand) bit it has just one part in it............ am I missing something big or did i just waste £805?

  • Cancel

Top Replies

  • e14softwareuk
    e14softwareuk over 9 years ago in reply to johnmosborneuk +3
    Hi John. Not sure if you are aware but in addition to the online Vault a vast collection of component libraries are available from the Altium website. Although not as convenient to access as the online…
  • Sparkylabs
    Sparkylabs over 9 years ago in reply to michaelwylie +2
    I am afraid that does not count as a libray, it has 3x 1K resistors, most through hole, one small SMD and one large SMD, not helpful. So I have to create every component from scratch, We are talking about…
  • bugrobotics
    bugrobotics over 9 years ago +2
    Hi Simon, It will probably be worth while to make your own libraries with the common components you use. Takes a few hours to get a bunch of standard components built but you can make them how you like…
Parents
  • michaelwylie
    michaelwylie over 9 years ago

    Place a part. Select Choose on the window that opens. Browse libraries will open. Choose Miscellaneous Devices. Should find the basic devices there.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • Sparkylabs
    Sparkylabs over 9 years ago in reply to michaelwylie

    I am afraid that does not count as a libray, it has 3x 1K resistors, most through hole, one small SMD and one large SMD, not helpful. So I have to create every component from scratch, We are talking about here for every value:

     

    Package size option: x2 (1205, 0805)

    Tolerance: x2 (1%, 0.1%)

    every resistor value and that is 4 options of every value. I'm offering to prostitute myself to farnell and lock myself into their brand if they supply a library, apparently beyond selling CS they have missed every other marketing opportunity. Oddly I have a farnell datapack installed somewhere but no idea what to do with it and it sounds like I have to manually create a library of parts to which apply that data.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
Reply
  • Sparkylabs
    Sparkylabs over 9 years ago in reply to michaelwylie

    I am afraid that does not count as a libray, it has 3x 1K resistors, most through hole, one small SMD and one large SMD, not helpful. So I have to create every component from scratch, We are talking about here for every value:

     

    Package size option: x2 (1205, 0805)

    Tolerance: x2 (1%, 0.1%)

    every resistor value and that is 4 options of every value. I'm offering to prostitute myself to farnell and lock myself into their brand if they supply a library, apparently beyond selling CS they have missed every other marketing opportunity. Oddly I have a farnell datapack installed somewhere but no idea what to do with it and it sounds like I have to manually create a library of parts to which apply that data.