Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Blog Staying Connected When Always on the Move - The Communication Backbone of Mobile Robots
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: SarahCrowe28
  • Date Created: 19 May 2026 4:35 PM Date Created
  • Views 1613 views
  • Likes 3 likes
  • Comments 0 comments
  • ADI Mobile Robotics
  • gmsl
  • Gigabit Multimedia Serial LinkTM (GMSL)
  • Motor and Control
  • ethernet
  • robotics
  • autonomous mobile robot
  • Motors & Motion Control
  • industrial automation
Related
Recommended

Staying Connected When Always on the Move - The Communication Backbone of Mobile Robots

SarahCrowe28
SarahCrowe28
19 May 2026
A factory scene featuring a cart on a robot, highlighting automation in an industrial environment.

by Rafael Marengo

We discussed how mobile robots navigate their environments through a variety of sensor types to collect data about the real world in the previous blog. However, we didn't explore how this data is communicated within the robot to translate perception into actions, such as movement.

Mobile robots consist of various technologies that must communicate with each other quickly and reliably to transmit critical messages for navigation and performing tasks, whether it's an Autonomous Mobile Robot (AMR) or an Automated Guided Vehicle (AGV). For a refresher on the differences between these types of robots, you can refer to this this blog in the series. Let’s consider the architecture of an AMR as shown:

image

Figure 1. AMR Communication Overview

There are several components that make up any mobile robot (such as wheel drive & encoder systems, vision inputs, inertial measurement unit (IMU) data, and battery management systems), and all of them need to communicate, usually with a main controller or main compute unit or sometimes to decentralized units that control specific functions of the robot, which can be done to reduce the overhead on a main controller and also aid in time critical applications such as  perception of its environment and actuator control. There are many communication methods that live within the operation of a typical mobile robot, and each type of protocol has their pros and cons for use. In the above example there are potentially 7 different communication methods employed within the one mobile robot: GMSL, UART, CAN, Ethernet, RS-485, SPI, RS-422. While this blog focuses on wired communication protocols, it is important to note that mobile robots typically require wireless communication as well. Wireless communication is essential for enabling mobile robots to interact with a base station and collaborate with other robots, ensuring seamless coordination and operation in dynamic environments.

Here is a quick comparison of a selection of technologies comparing their speed and latency.

image

As it can be seen in table 1, the parameters for the highlighted technologies vary in speed and latency and the appropriate technology needs to be chosen according to the need and the design itself and will most likely include a combination of different technologies. Operations in mobile robots typically demand near real-time speeds to function effectively. This is crucial for tasks such as obstacle avoidance, navigation, and interaction with dynamic environments, where even slight delays can impact performance and safety. The key parameters that need to be taken into consideration for communication are performance, reliability, and scalability.

An AMR needs to be able to navigate while perceiving its surroundings to execute tasks in an efficient way, and a simple flow diagram can describe how it acts:

image

Both the perception and the action parts play important roles, the environment needs to be perceived in order for actions to be taken and this data is usually acquired with RGB cameras, depth cameras, Lidar sensors and radar or a combination but transferring all this data to a processing unit needs a robust link with enough bandwidth and in the case of industrial robots, reliability against interferences. That critical work can be executed by protocols such as GMSL.

Gigabit Multimedia Serial Link

There is a new protocol entering the mobile robotics scene, GMSL. The protocol can transfer up to 6 Gbps of advanced driver assistance systems (ADAS) sensor data over a coax cable while simultaneously transferring power and control data over a reverse channel. It is a highly configurable serializer deserializer (SERDES) interconnect solution which supports sensor data aggregation (Video, LiDAR, Radar, etc.), video splitting, low latency and low bit error, and Power over Coax (PoC)

The topology for a GMSL application consists of the sensor, a serializer, a cable, and a deserializer on the system on chip (SoC) side.

image

This simplifies the mobile robot design and makes it more robust since GMSL was designed with transferring this type of data and was optimized to ensure high bandwidth, low latency transmission of data.

The synergy between Industrial Ethernet, GMSL, and wireless communication technologies is driving the next generation of mobile robotics. These technologies provide the robust, high-speed, and flexible communication necessary for mobile robots to operate autonomously and efficiently in various environments. As innovations continue to emerge, the capabilities of mobile robots will expand, revolutionizing industries and transforming our daily lives. To learn more, visit analog.com/mobile-robotics.

WIRED COMMUNICATION 

MAX96724RGTN/V+T

AD-GMSL522-SL Evaluation Kit

MAX96717R-AAK-EVK# Evaluation Kit

EVAL-ADIN1110EBZ Eval Kit  ADIN1110BCPZ  ADIN1110CCPZ

DEMO-ADIN1100D2Z Evaluation Kit   EVAL-SPOE-KIT-AZ Evaluation Kit  ADIN1100BCPZ   ADIN1100CCPZ   EVAL-ADIN1100EBZ

EVAL-ADIN1200FMCZ Evaluation Kit  EVAL-10BT1L-MCS-BZ Evaluation Kit  EVAL-10BT1L-MCS-AZ Evaluation Kit  ADIN1200BCP32Z

EVAL-ADIN1300FMCZ Evaluation Kit  EVAL-CN0506-FMCZ  ADIN1300CCPZ  ADIN1300BCPZ

WIRELESS COMMUNICATION

HMC7044LP10BE

HMC7044LP10BETR

EK1HMC7044LP10B Evaluation Kit