BitScope
  • Products & Partners
  • Manufacturers
  • BitScope
  • More
  • Cancel
BitScope
Forum Hardware troubleshooting BitScope 442N Rev 3
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BitScope to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 36 subscribers
  • Views 131 views
  • Users 0 members are here
  • bitscope
Related

Hardware troubleshooting BitScope 442N Rev 3

billmania
billmania 2 months ago

I have serial BS44501-1409003. The board is labeled "Bitscope 442N Rev 3". It has two removable modules. The first is labeled "BitScope Network Controller LIA BootLoad" and the second is "BitScope VM-445N (C) 2008 Metachip".

The symptoms of the board are:

- the external power LED is lit steady

- at power up, the Data LED blinks and then stays off

- at power up, the Link LED lights after a few seconds, and stays lit

- sending UDP multicast 230.10.10.10 port 16385 on the LAN does NOT blink the Data LED

- no network traffic is emitted by the BitScope

- other hosts on the same LAN do receive the UDP multicast datagrams

- X1 pin 1 has 5 VDC

- X1 pin 5 has 5 VDC

I have at least three questions:

1. how can I get a schematic for this board

2. what is the manual "force reset" mechanism for this board

3. what are the definitions of the 7 pins at X1

  • Sign in to reply
  • Cancel
Parents
  • billmania
    0 billmania 2 months ago

    After much effort expended, I've confirmed incoming multicast datagrams are at least reaching the RTL8019AS. This was determined by observing 5 Volt square wave pulses on the RTL8019AS's pin 12 (Rx), synchronized with the datagram transmission. At the same time, The RTL8019AS's pin 13 (Tx) never budged from 0 Volts. Pin 13 is connected to Q1, which is in turn connected to R12, which finally connects to the DATA LED's minus lead.

    Of my three questions in the original post, 2 and 3 are now irrelevant. A schematic would still be really helpful. A troubleshooting procedure for the PIC18F 442 Network Controller would be nice, too. Otherwise, I have nothing more than some e-waste now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billmania
    0 billmania 2 months ago

    After much effort expended, I've confirmed incoming multicast datagrams are at least reaching the RTL8019AS. This was determined by observing 5 Volt square wave pulses on the RTL8019AS's pin 12 (Rx), synchronized with the datagram transmission. At the same time, The RTL8019AS's pin 13 (Tx) never budged from 0 Volts. Pin 13 is connected to Q1, which is in turn connected to R12, which finally connects to the DATA LED's minus lead.

    Of my three questions in the original post, 2 and 3 are now irrelevant. A schematic would still be really helpful. A troubleshooting procedure for the PIC18F 442 Network Controller would be nice, too. Otherwise, I have nothing more than some e-waste now.