Intelligent LED Solutions
  • Products
  • Manufacturers
  • Intelligent LED Solutions
  • More
  • Cancel
Intelligent LED Solutions
Blog Constant current versus constant voltage power supplies, with Inventronics
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intelligent LED Solutions to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sabrina.hobson
  • Date Created: 12 Dec 2023 9:18 AM Date Created
  • Views 903 views
  • Likes 2 likes
  • Comments 0 comments
Related
Recommended

Constant current versus constant voltage power supplies, with Inventronics

sabrina.hobson
sabrina.hobson
12 Dec 2023
Constant current versus constant voltage power supplies, with Inventronics

Constant current (CC) and constant voltage (CV) are two terms commonly heard when discussing LED drivers. These terms distinguish between the two available types of LED driver used in electronics, particularly in LED lighting and other electronic devices.

                                                                                                                                                                                                                                                                                                                                                                  

What is the difference?

The difference is paramount, and your LED application will determine the type of driver you need. The main difference lies in how they regulate and deliver electrical power to the connected load:

Constant Current (CC) Drivers: These drivers maintain a constant electric current output by having a variable voltage. Constant current drivers ensure that the current flowing through the load remains steady, even if the load's resistance changes. CC LED drivers tend to offer a more efficient circuit and better control, when compared to CV LED drivers.

Constant Voltage (CV) Drivers: On the other hand, constant voltage drivers supply a set voltage output to the electronic circuit. The current drawn by the load varies based on its resistance.

 In summary, constant current drivers are suited to applications where the load requires a fixed current. Whereas, constant voltage drivers are used when a steady voltage level is essential, allowing the current to vary based on the load's requirements. The choice between the two depends on the specific requirements of the electronic device or lighting system being powered.

  

Where are they used?

 Constant current LED drivers are a popular choice for LED applications and are suitable for use with LED chains or single LEDs operating in series. They are commonly used in applications where the load, such as LEDs, requires a consistent current for optimal performance and longevity.

While constant voltage LED drivers are ideal for a parallel circuit made up of multiple LEDs. Devices that require a fixed voltage input, such as some electronic gadgets and components, use constant voltage drivers to maintain a consistent voltage level across the load. They are best suited for LED modules with either an on board or a current limiting resistor, such as an LED strip. 

 

About Inventronics

NB: In May 2023, OSRAM sold its LED Drivers, Lighting Controls, LED Flex and LED Modules business to Inventronics. These products continue to be branded OSRAM but are now owned, designed, manufactured, and developed by Inventronics.