Intelligent LED Solutions
  • Products & Partners
  • Manufacturers
  • Intelligent LED Solutions
  • More
  • Cancel
Intelligent LED Solutions
Blog LED Drivers: All you need to know
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intelligent LED Solutions to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sabrina.hobson
  • Date Created: 31 May 2023 9:13 AM Date Created
  • Views 2299 views
  • Likes 7 likes
  • Comments 2 comments
  • LED driver
  • osram
  • power supply
  • lighting
  • led
  • ILS
Related
Recommended

LED Drivers: All you need to know

sabrina.hobson
sabrina.hobson
31 May 2023
Multiple LED power supply of varying size, shapes and colours from the ILS and OSRAM brands

What to consider when choosing an LED driver:

 

Constant current (CC) or Constant voltage (CV)

Depending on your LED modules and application you may require CV or CC.

  • CC LED drivers are a popular choice for LED applications and are suitable for use with LED chains or single LEDs operating in series. Series refers to multiple LEDs mounted and linked together with the current flowing through them all. Within a series, if the circuit is not broken, all LEDs will receive current and operate as expected. However, if the circuit is broken, none of the LEDs will be powered. CC LED drivers keep a constant electric current throughout an electric circuit by having a variable voltage. In comparison to constant voltage CC LED drivers tend to offer a more efficient circuit and better control.
  • CV LED drivers, on the other hand, supply a set voltage to the electronic circuit. CV LED drivers are ideal for a parallel circuit made up of multiple LEDs. For example, they are best suited for LED modules with either an on board or a current limiting resistor, such as an LED strip. The voltage requirement of the entire LED chain must match the voltage output of the CV LED driver.

 

IP Rating 

For an LED driver to be used outdoors, an IP rating of IP65 is required. Likewise, if the application requires a driver that can be submerged in water, IP67/IP68 will be needed. Alternatively, if the application is indoors and the LED driver does not need protection from the elements, a driver IP rating of IP20 would be suitable.

Dimming 

Your LED module and application may need to dim the brightness of the LEDs. Dimming is possible via several methods. These include:

  • 0-10Volts - For direct current voltage (DC) between 0 and 10 volts.
    This can produce light at varying intensity levels. 0-10V dimming is the simplest control system for lighting, providing smooth operation and dimming down to 10%, 1%, and even 0.1% light level.
  • Mains dim - Phase cut, triac dimming, leading edge, or trailing edge.
    This reduces the electrical energy level flowing through the LEDs, thereby causing them to dim.
  • Pulse-width modulation (PWM) - A common type of dimming used to adjust the current in white-LED driver devices.
    PWM dimming takes a rectangle waveform with a variable positive duty cycle and adjusts the LED current proportionally.
  • Dali - These dimmer switches use a digital protocol to send a dimming control signal to a driver down separate wires to the mains supply. They do not directly control the energy passed to the driver. 

 

Wireless

This works by sending wireless signals through your home Wi-Fi or mesh network.
These wireless switches can control lighting, ceiling fans or anything connected to the switch, including adjusting the brightness of your lights.

 

Output current 

Your driver’s output current needs to match the requirements of the LED you are driving. I.e., if your LEDs need 350mA then your LED drivers output needs to be 350mA also. Output current is a value given in amps (A) or milliamps (mA). 1000mA make up 1A. To use a CC driver, make sure to check the current requirements of your chosen LED(s). This can typically be found within the LED’s datasheet.

Your LED’s required current must match or fall within the output current range of the CC LED driver. Using a higher current than recommended for the LED will wear the LED out a lot quicker, reducing its lifetime. Whereas running the LED at a lower current would have the opposite effect.

 

Output power 

Measured in Watts (W), the LED driver you choose should have an output power that is at least the same value as your LED’s power requirements. Ideally though, the output power should be higher than the LED’s power needs. This is because if the driver’s maximum output is equal to the power requirements of the LED, then the driver will be operating at full power. This may shorten the LED driver’s life span.

Secondly, the power requirement of the LEDs tends to be calculated as an average, with tolerance added on top for multiple LEDs, so ideally you should have a higher output power from the driver to factor this in.

 

Output voltage 

Measured in Volts (V), referring to the voltage produced by the LED driver and supplied to the chosen LED(s). For CC LED Drivers, the output voltage needs to exceed the voltage requirements of the entire chain of LEDs you are trying to drive. For CV LED drivers, the voltage required by your LEDs needs to match the output voltage of the LED driver.


Dimensions 

Make sure the LED driver you chose fits any space limitations you may have.

 

Lifetime

All LED drivers tend to come with a lifetime expectancy of thousands of hours. This value is known as MTBF, which is the ‘mean time before failure’. To extend the lifetime and reduce maintenance costs and time, make sure to run your chosen LED driver with the recommended outputs.

 

Suggested Products

The ILS team is here to help you select the optimal LED driver for your project. We offer a variety of OSRAM DS power supplies, as well as our own ILS power supply product range.

  • IZC035-004F-4065C-SAL – ILS Constant Current LED Driver, 4W, 100V, 350mA, IP65
  • IT-FIT-4/220-240/400-CS-I – OSRAM ICUTRONIC FIT Compact Constant Current LED Driver, Non-dimmable
  • OTi-DALI-10/220-240/700-NFC-I – OSRAM OPTOTRONIC Intelligent Compact Constant Current LED Driver, Dimmable
  • OT-SLIM-60/220-240/24  – OSRAM Constant Voltage LED Driver 24V, 60W

 

  • Sign in to reply
  • sabrina.hobson
    sabrina.hobson over 3 years ago in reply to robogary

    Yes the LED type and parameters will be absolutely key in determining what LED driver can be used. A COB LED is just like any other LED, it will still require a current and voltage to run. How much current and volts the COB requires, will depend on the size. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 3 years ago

    The choice depends alot on the led selected.

    Neopixels need CV. Power Leds >1 watt I like having both volts and amps adjustable. COB  leds I don't understand their ckts enough to say CV for sure.