Intelligent LED Solutions
  • Products & Partners
  • Manufacturers
  • Intelligent LED Solutions
  • More
  • Cancel
Intelligent LED Solutions
Blog LED optics: lenses versus reflectors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intelligent LED Solutions to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sabrina.hobson
  • Date Created: 12 Mar 2024 2:19 PM Date Created
  • Views 1689 views
  • Likes 5 likes
  • Comments 1 comment
  • reflector
  • lens
  • osram
  • lighting
  • optic
  • led
  • ILS
  • LEDiL
Related
Recommended

LED optics: lenses versus reflectors

sabrina.hobson
sabrina.hobson
12 Mar 2024
LED optics: lenses versus reflectors

LED optics are a terrific way to direct, diffuse or intensify light. They are readily available in a wide array of sizes, shapes, and materials. This variety of choice means that lenses are versatile and useful in many different applications.

Lenses

Lenses can be used on single LED or multiple LED modules, as well as visible or non-visible light (infrared and ultraviolet). They are typically made from polycarbonate (PC) or polymethylmethacrylate (PMMA). The end application will ultimately determine the suitability of the material. For example, in UV applications, a silicone lens would be required, as this material will not be affected by the UV wavelengths.

Lenses work by refracting the light passing through. A convex lens will target light to one focal point, creating a narrower beam. Whilst a concave lens will project light into a wide angle, increasing coverage.

image

The benefits…

Lenses are a fantastic way to enable precise control over light output and produce a desired lighting effect. They can create different beam angles to suit many applications and tend to excel as a solution for indoor settings where visual excellence and precision are required. Lenses can collimate light into a concentrated narrow beam, ideal for spot or accent lighting. Thus, lenses are beneficial to increase light control, direction, and intensity.

In doing so, they also reduce unwanted glare and create a more refined and seamless light effect. Which also has its benefits as by reducing light wastage through illuminating unrequired areas, energy efficiency is improved.

Using a lens will also give the lighting fixture a more pleasing appearance, as the raw LED and PCB can be effectively concealed.

Reflectors

As with LED lenses, reflectors sit over an LED to alter the beam of light. They are also available in a variety of sizes and materials. Most commonly reflectors are made from plastic and metal coated to increase the reflective capabilities. The surface reflecting light can be multifaceted or smooth to create various lighting effects. The angle of light dispersal will also be determined by the reflector shape. For example, to create a narrower beam, typically a larger optic is needed. Therefore, reflectors are best suited to applications where light needs dispersing across a wide area, rather than applications needing a direct focused beam.

image

The benefits…

Reflectors are a popular solution for general lighting applications where precision is not a key concern. They are a cost-effective and easy to implement. They are implemented in most incandescent lights, but they also can be beneficial in LED lighting applications too. Their effectiveness in directing light evenly paired with their cost-effectiveness, make reflectors an ideal solution for many general lighting applications, particularly where budgets are a consideration.

We strongly recommend LEDiL secondary optics for the best solutions. ILS (Intelligent LED Solutions) is a franchised distributor of LEDiL products, and designs complementary LED modules to work seamlessly with the LEDiL optics range.

image


  • Sign in to reply
  • DAB
    DAB over 2 years ago

    There is a loss of transmission through lenses.

    We used to estimate about 6% loss per glass element.

    I do not know if the plastic lenses have similar characteristics.