KEYSIGHT TECHNOLOGIES
  • Products & Partners
  • Manufacturers
  • KEYSIGHT TECHNOLOGIES
  • More
  • Cancel
KEYSIGHT TECHNOLOGIES
Forum component testing with keysight dsox1102g scope
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join KEYSIGHT TECHNOLOGIES to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 40 replies
  • Answers 25 answers
  • Subscribers 22 subscribers
  • Views 7974 views
  • Users 0 members are here
  • component tester
  • elenco
  • short
Related

component testing with keysight dsox1102g scope

johnwater
johnwater over 6 years ago

hello would like to learn how to measure components on my elenco am radio kit.

am new to electronics, trying to figure things out.

read about lissajous patterns, just need some direction as to how to set up my connections, see if components are functioning as necessary.

my 9 volt battery gets hot, no audio output,so  i think i have short somewhere?

thanks

john

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to johnwater +4 suggested
    The soldering is good. I see that most of the transistors are NPN. There's 2 PNPs that I can see (Q5, Q7). You have different part numbers for those? Electrolytic capacitors look correct (I can't see the…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +4 suggested
    Looking at the potentiometer, it seems that it has been inserted from the wrong side (inserted from above instead of pushed in from the underside).. The movable switch part looks forced (blue), and the…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to fmilburn +4 suggested
    I think that the second pin of the switch is soldered to the wrong hole:
Parents
  • Jan Cumps
    0 Jan Cumps over 6 years ago

    ... also, does the documentation say when you should plece the wire J1?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 6 years ago in reply to Jan Cumps

    It looks like J1 is supposed to be installed

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnwater
    0 johnwater over 6 years ago in reply to fmilburn

    not seeing anything about a J1 in assembly, looks like they just leave it empty.

    john

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 6 years ago in reply to johnwater

    J1 is the jumper wire on page 8 of the instructions - it looks like you installed it

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnwater
    0 johnwater over 6 years ago in reply to johnwater

    sorry my mistake, there is a J1.

    now i need to see where that goes.

    john

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to fmilburn

    I think that the second pin of the switch is soldered to the wrong hole:

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnwater
    0 johnwater over 6 years ago in reply to Jan Cumps

    Thanks Jan

    i see your drawing.

    lots of questions re this switch.

    I will de solder, take it off ,take some pics, then desolder and check.

    With my vom one of the pins was bent toward the housing of the switch, should be separate and part,so i have created a short.

    gonna straighten things out and repost some images.

    john

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Jan Cumps

    The pins that are southbound in that photo snippet belong to a couple of capacitors, connected to ground : ( And that's the same copper area near the switch. Hot battery issue root cause solved I guess!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnwater
    0 johnwater over 6 years ago in reply to johnwater

    took switch off, looked at connection points.

    still not sure that what is circled in blue is correct slot.

    i think these boards are made generic for other radios as wetland that slot seems to be  way off to the side.

    took pics of top and bottom of board.

    definitely had a part of pot on /off blade touching the base of pots i unbent it and straightened it out.

    gonna desolder everything and get back to u all.

    slot i circled in red appears to need to stay open, it just would be too outside the pot pins, may be for some other project.image

    thanks for all the help.better eyes than mine found a problem.

    johnpot imageimage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to johnwater

    Hi John,

     

    The switch terminal cannot go in the nearer slot, because that area of copper connects to ground, you can follow it to the negative terminals of capacitors for example, and if the switch is connected to ground, that's a short to ground.

    I agree it's confusing, but that nearer slot is likely for a different potentiometer/switch, where perhaps the shell has a locating peg that could be soldered there.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to shabaz

    Yes, it has to go in the outer hole, sharing the copper trace with C14+ and jumper J1. The closer hole is for potentiometers that have a small hook on the housing to keep them oriented correctly.

     

    In the instruction manual, you can see that the 2 switch pins are bent outward.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnwater
    0 johnwater over 6 years ago in reply to shabaz

    he's the pot shell bas e does have a small tab on bottoms guess that should fit it the closest slot.but not sure it should be soldered?as it is underneath the base, hard to get to.the instructions not to solder 5 lugs' guess 3 wipers and 2 switch lugs, no mention of the small tab.

    thanks

    john

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnwater
    0 johnwater over 6 years ago in reply to shabaz

    he's the pot shell bas e does have a small tab on bottoms guess that should fit it the closest slot.but not sure it should be soldered?as it is underneath the base, hard to get to.the instructions not to solder 5 lugs' guess 3 wipers and 2 switch lugs, no mention of the small tab.

    thanks

    john

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 6 years ago in reply to johnwater

    Hi John,

     

    It (mostly) doesn't matter electrically. As you say, it's just a 3 terminal potentiometer, and a switch. You can use judgement to determine if that lug needs soldering or not (e.g. based on how physically strong it is, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to johnwater

    the small tab should not be soldered.

     

    edit: some background on that:

     

    All the contacts are made of a compliant metal. When force is put on the potentiometer, the flex in the leads will absorb it and little force goes to the solder pad.

    The tab is made of hard iron and its role is to physically prevent rotation/slip. It's non-compliant, and any force on it is directly transferred to the sides of the hole it's mounted in.

    If you solder this, slip force will be put on the (weak by nature) solder joint. It either will crack or tear the pad off the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer