Moto Mods
  • Products
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Forum Anything special to get USB to work on the side of the case?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 6 answers
  • Subscribers 59 subscribers
  • Views 2832 views
  • Users 0 members are here
Related

Anything special to get USB to work on the side of the case?

garengllc
garengllc over 9 years ago

I have a Moto Z and was hoping to connect an RTL-SDR dongle to the side of the proto case.  I attempted to setup the dip switches to enable the USB 3.1 interface and connected a USB OTG cable, but the phone is still not recognizing the device (I am using the middle USB connection).  Is there something else that I am missing?

  • Sign in to reply
  • Cancel

Top Replies

  • flowflow25
    flowflow25 over 9 years ago in reply to anttibrain +2 suggested
    Some notes on USB to try and answer several of the questions here. USB3 is literally just that, the USB3 PHY. It does not include the additional lines for USB2 (those have their own dedicated interface…
  • anttibrain
    anttibrain over 9 years ago +1 suggested
    Please read the documents the switches you need are the A3/A4 the USB 3.1 switches are not relevant if you want to use RTL dongle that is pure USB2 device. Unfortunatly I can not test anything here as…
  • michaelkellett
    michaelkellett over 9 years ago in reply to anttibrain +1
    I'm interested in the FPGA side of things but not into the moto-z. My application for TE0725 is to do prototyping for new designs where we will use Artix FPGA (probably 100 size) and also for use in test…
Parents
  • msp
    0 msp over 9 years ago

    I am having the same issue.  Is it just a matter of setting the dip switches correctly or do I need a custom firmware? I have tried setting up the development environment  but keep getting the no valid JTAG interface. Is there a ready to flash firmware somewhere that will enable the usb ports?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • flowflow25
    0 flowflow25 over 9 years ago in reply to msp

    USB2.0 or USB3.1?

    TypeC (USB#2) port or MicroB (USB#3)?

    Did you put yourself into Developer mode and build and flash the compute (USB3.1) or usb2 (USB2.0) example in the nuttx repo?  There isn't a 'ready to flash' but they are certainly ready to build.  And the power changes mentioned in my previous message have already been pushed so no code changes should be necessary (you may need to re-pull).

    Are you using an OTG cable?

     

    As far as the development environment, did you perform the steps needed to provide permissions (see OpenOCD here)?  Are you plugging into the top TypeC port on the MDK?

    Dip switch settings will depending on the answer to the first 2 questions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • flowflow25
    0 flowflow25 over 9 years ago in reply to msp

    USB2.0 or USB3.1?

    TypeC (USB#2) port or MicroB (USB#3)?

    Did you put yourself into Developer mode and build and flash the compute (USB3.1) or usb2 (USB2.0) example in the nuttx repo?  There isn't a 'ready to flash' but they are certainly ready to build.  And the power changes mentioned in my previous message have already been pushed so no code changes should be necessary (you may need to re-pull).

    Are you using an OTG cable?

     

    As far as the development environment, did you perform the steps needed to provide permissions (see OpenOCD here)?  Are you plugging into the top TypeC port on the MDK?

    Dip switch settings will depending on the answer to the first 2 questions.