Moto Mods
  • Products & Partners
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Forum Using USB firmware to give two USB ports?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 58 subscribers
  • Views 960 views
  • Users 0 members are here
Related

Using USB firmware to give two USB ports?

j_warner
j_warner over 9 years ago

Using the usb2 firmware is it possible to have two different USB devices connected, one to the phones port, and one to one of the MDK ports?

 

Thanks,

James

  • Sign in to reply
  • Cancel
Parents
  • motomodsdev
    0 motomodsdev over 9 years ago

    Unfortunately, no.  You can charge from the TypeC on the MotoZ, but you cannot have simultaneous data with Mod USB.

    Due to this and power concerns, it is critical to disable Mod USB when not in use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nampu
    0 nampu over 9 years ago in reply to motomodsdev

    Is it possible to have two usb devices connected to each of the ports on the MDK ? The Type C port on the moto Z will to be used only for charging.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • motomodsdev
    0 motomodsdev over 9 years ago in reply to nampu

    With the MDK you can use USB#2 (Type C) for powering your prototype, B4 should be OFF (and probably B3 unless you have battery/charging on your prototype).

    Then you'd set A3=ON, A4=OFF to bring data to the USB#3 (MicroUSB) port.  With the usb2 firmware, the microUSB port is always powered.  That said, the usb2 sample firmware was started from base_unpowered and does not contain Battery/PTP so it will not push/pull power from the MotoZ.

     

    In your actual Moto Mod product, if you need multiple USB devices then you would place a hub in your Mod.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adamk
    0 adamk over 8 years ago in reply to motomodsdev

    how do i configure the mod to allow usb host from the mod and have the mod charge the phone at the same time?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • adamk
    0 adamk over 8 years ago in reply to motomodsdev

    how do i configure the mod to allow usb host from the mod and have the mod charge the phone at the same time?