Panasonic
  • Products
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Forum HAVE A QUESTION ON CAPACITORS,ASK AN EXPERT!
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 48 replies
  • Subscribers 29 subscribers
  • Views 6723 views
  • Users 0 members are here
  • capacitor
  • expert
  • panasonic
Related

HAVE A QUESTION ON CAPACITORS,ASK AN EXPERT!

Resistor+caps
Resistor+caps over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Passive in the element14 Community Passive group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


 

 


  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 12 years ago

    What happens to an Aluminum Electrolytic Capacitor when it is used below its rated temperature. Let's say we have an 180uF cap rated at 450V and the unit that it is installed in drops to below the -40C rating. Does the the capacity (uF) decrease? Does the part explode/disintegrate? Is the part ruined or otherwise rendered disfunctional? What will happen to our power supply's capacitors when it is used in temperatures that are lower than the rated temperatures?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jing.liu
    jing.liu over 12 years ago in reply to Former Member

    Dear Richard

     

    Panasonic Aluminum Electrolytic Capacitors with middle /high voltage (160V and above) are featuring temperature range down to -25 degreeC.

    The ESR will increase and capacitance will decrease more at low temperatures below -25degreeC for such high voltage capacitors.

     

    I can show you here per attached techincal data which is available, reflecting temperature characterisctics of 450V /47uF (through hole type).

     

    hope it's helpful for you!

     

    Best regards,

    Jing

    Attachments:
    imageA-EE-450V-47uF-EEUEE2W470S_temp_charac.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jing.liu
    jing.liu over 12 years ago in reply to Former Member

    Dear Richard

     

    Panasonic Aluminum Electrolytic Capacitors with middle /high voltage (160V and above) are featuring temperature range down to -25 degreeC.

    The ESR will increase and capacitance will decrease more at low temperatures below -25degreeC for such high voltage capacitors.

     

    I can show you here per attached techincal data which is available, reflecting temperature characterisctics of 450V /47uF (through hole type).

     

    hope it's helpful for you!

     

    Best regards,

    Jing

    Attachments:
    imageA-EE-450V-47uF-EEUEE2W470S_temp_charac.pdf