Würth Elektronik
  • Products & Partners
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog EMC Basics: Common Mode vs. Differential Noise
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Würth Elektronik
  • Date Created: 27 Nov 2023 9:15 AM Date Created
  • Views 3355 views
  • Likes 10 likes
  • Comments 1 comment
  • emc
  • würth elektronik
  • wurth_elektronik
Related
Recommended

EMC Basics: Common Mode vs. Differential Noise

Würth Elektronik
Würth Elektronik
27 Nov 2023
EMC Basics: Common Mode vs. Differential Noise

EMC Basics: Common Mode vs. Differential Noiseimage

Author: Dheeraj Jain, Technology Strategist; Jenna Cummins

Today, we will talk about the differences between common mode and differential noise in EMC and how to combat them.

Common Mode vs. Differential Noise

As a quick reminder, differential currents flow in opposite directions through the source and return path, while common mode currents flow the same direction through the source and return path, completing the circuit through the ground path.

 image   image

Differential mode noise path                                                                                   Common mode noise path

Figure 1. Differential mode and common mode noise paths

How to know if you are dealing with common mode noise or differential noise? This is a common question that needs to be answered.

Here's a quick trick to getting you headed in the right direction. While it's not 100% accurate, it helps get the process started.

Imagine a doctor prescribing antibiotics without knowing whether you have a bacterial infection or a virus. He does so knowing that if you have a bacterial infection, the medication will work, and the problem will be solved. If the medication does not work, at least he knows he’s dealing with a virus, and will then treat you accordingly.

So in our case, you can simply apply a clamp-on ferrite onto a cable, remembering both lines (Vcc and ground) will be in that cable. If the noise is reduced (or the immunity is increased) then you’re experiencing a common mode problem. If there's no effect, it’s a differential mode problem.

Therefore, at the board level, if it is a common mode problem, you can use a common mode choke. If the problem is differential mode, a chip bead ferrite can be used.

Material Characteristics

Clamp-on ferrites are typically made with two different types of materials: manganese zinc (MnZn) and nickel zinc (NiZn).

Nickel zinc can be used in situations with either conducted or radiated noise at high frequencies. Manganese zinc is mostly used for conductive noise at lower frequencies because its higher permeability gives more impedance.

This image provides a guideline for which material to use depending on your situation. Of course, there are exceptions, but this is what we find to be typical.

image

Figure 2. Materials for clamp-on ferrites, where conducted and radiated immunity are tested and the common frequency range where differential and common mode noise occur.

Reducing Common Mode Noise

Here, we have a visual representation of how a common mode choke works.

image

Figure 3. Common mode vs. Differential signals

The red arrows represent a differential signal going in. This is the useful signal. It creates a magnetic field inside the core going in one direction, according to the right-hand rule.

The differential signal then goes back to the source, which creates another magnetic field, according to the right-hand rule. These two fields will cancel each other in the core.

Common mode noise also creates a magnetic flux inside the core, but this time both noise signals are in the same direction, as shown here by the black arrows resulting in the magnetic fields adding together. The core will response with high impedance to the unwanted noise.

When the Signal Will Be Attenuated

Something to keep in mind when using a common mode filter is that there will be a differential impedance that could attenuate the useful signal. As shown in the graph in Figure 6, the blue line represents the common mode impedance, and the red dotted line shows the differential impedance.

image

Figure 6. Common mode and differential impedance of a typical common mode inductor.

This means if the signal is at 100 MHz, using this common mode solution, there will be some unintentional attenuation of the signal from the differential impedance.

The Best Solution to Filter Noise Close to Signal Frequency

Here is a specific example. The blue line represents the common mode impedance, and the red dotted line shows the differential mode impedance. The useful signal is shown by the thick black line right at 4 MHz.

image

Figure 7. Avoiding impact on useful signal

This is making good use of the common mode chokes, with a high common mode impedance right at that 4 MHz and a low differential mode impedance.

Therefore, the impact on the noise is high, and the impact on the useful signal is kept to a minimum. When reading the datasheets, check both the common mode impedance and the differential mode impedance for that part.

Sectional vs. Bifilar Windings

There are two types of windings used in a common mode choke: sectional and bifilar.

image

image

image

Figure 8. Sectional vs. Bifilar Winding

Sectional-wound components are most useful in power supply applications because high voltage lines must be separated by a minimum distance. They can also be used as inductors to attenuate differential mode noise. Because sectional components have a higher leakage inductance, they attenuate differential mode noise as well as common mode noise.

Bifilar-wound parts are typically used for low voltage data signal lines because we don't want to attenuate the differential mode signal (useful signal). Thus, you have a lower leakage inductance, and that is utilized for filtering noise on a signal.

To summarize, the way either parts attenuate common mode noise is very similar. However, there’s a big difference between sectional-wound and bifilar-wound parts when it comes to differential mode noise attenuation.

You can see these differences shown with the red and black lines Figure 8. Notice that the common mode impedance (solid lines) are very similar, whereas the differential mode impedance (dashed lines) are very different.

CMC Selection via REDEXPERT

Würth Elektronik’s online tool REDEXPERT can help you find the right components to attenuate noise. Use REDEXPERT’s EMI Filter Designer to help design and visualize the results. Simply enter the details of the system and the noise you are looking to attenuate in order to find the proper components.

By understanding the difference between common mode and differential noise, as well as how to use common mode chokes, you will be able to reduce unwanted noise in your designs. Our next article will provide even more information on differential noise and chip bead ferrites, so be on the lookout to keep improving your EMC knowledge!

In the meantime, our previous articles on EMI Basics and EMC Losses are also available.

  • Sign in to reply
  • DAB
    DAB over 2 years ago

    Nice overview of the issues with noise and how to cancel it.